FD30 Across-the-Line

FD30 Across-the-Line

The FD30 controller operates Across-The-Line where full voltage is applied to the motor for starting by the use of a single motor contactor. Starting inrush current is approximately 600% of rated full load amperes. The FD30 can be programmed for either fully automatic or semiautomatic operation.