MRR1000 Remote Racking Device
FINALIST - Plant Engineering's 2011 Product of the Year
The MRR1000 permits the operator to open and close a breaker from up to 25 feet away during the rack-in or rack-out process, well beyond the arc flash boundary for LV switchgear. Protecting personnel from the dangers of potential arc flash occurrences demand greater distance between an operator and the front of a switchgear lineup during racking operations.
The MRR1000 permits the operator to open and close a breaker from up to 25 feet away during the rack-in or rack-out process, well beyond the arc flash boundary for LV switchgear. Protecting personnel from the dangers of potential arc flash occurrences demand greater distance between an operator and the front of a switchgear lineup during racking operations.
Works with all breakers in the Magnum DS family (MDS, MDN, SBS, SBN, and CM52)- Locking fixture mounts directly to Magnum DS breaker escutcheon
- 25-foot umbilical cord between operator and device
- Ready lights indicating power to the unit and pendant
- Complete racking in 25 seconds or less
Loading Content..Please wait!