Addressable Relay II
The Addressable Relay II is designed for use where remote control of information or non-communicating devices is required. The relays communicate at 9600/1200 baud on the Eaton PowerNet system. Devices are assigned a three-digit address to uniquely identify them on the daisy-chained twisted shielded pair network.
- Communications watchdog feature monitors communications between the Addressable Relay II and the computer control station; if communications are lost, the communications watchdog will reset the relay to the de-energized (OFF) state.
- Includes two status indicating circuits (IN1 and IN2) which can be used to transmit the contact status of devices external to the Addressable Relay II.
- Each input is isolated with its own return.
Loading Content..Please wait!