Arc Resistant Gear

Arc Resistant Gear

ANSI/IEEE C37.20.7 defines switchgear arc resistance in two basic categories:

  • ANSI type 1
    Arc resistance from the front of gear only
  • ANSI type 2
    Arc resistance provided from the front, sides and rear

A suffix may be added to either of these two types to further define the type of protection provided:

  • A: Basic design
  • B: Arc resistance is maintained even while opening designated low voltage compartments
  • C: Arc resistance is maintained even when opening designated adjacent compartments
  • D: Special designation that supplements the Type 1 designation, but identifies additional arc resistance in certain structures

Eaton offers arc resistant medium voltage (MV),and low voltage (LV) switchgear and arc resistance MV motor control. Eaton also offers a unique “arc preventative” LV motor control center (FlashGard) that protects the operator by reducing the likelihood that an arc would occur.