White Papers
Eaton's white papers demonstrate how our technology solutions can best address your needs and solve your most pressing business problems.
| Title | Publication Date
|
Type | Size |
| The ABCs of UPS Service
Eaton Corporation, a global leader in power quality, distribution and control, recommends the inclusion of a service plan in order to maximize the performance and reliability of an uninterruptible power system (UPS). This white paper examines the basic concepts of UPS service. |
3/22/2009 |
|
38 KB |
| Choosing a UPS Service Plan
Eaton Corporation, a global leader in power quality, distribution and control, recommends the inclusion of a service plan in order to maximize the performance and reliability of an uninterruptible power system (UPS). This white paper examines the four primary options available for maintenance and service of UPS products and outlines the differences and specific advantages among these alternatives. |
3/22/2009 |
|
58 KB |
| The Benefits of a Preventive Maintenance Service Plan for your UPS
Because companies rely on a UPS to deliver continuous power without any disruption to their business, a maintenance plan is a critical component to ensure that a UPS minimizes the risks of downtime and performs as expected. |
3/22/2009 |
|
259 KB |
| Is your data center ready for virtualization?
Virtualization brings the potential to deliver dramatic savings in terms of server count, footprint, power consumption and cooling requirements for data centers. |
3/15/2009 |
|
498 KB |
| The necessary convergence of IT and Facilities
The necessary convergence of IT and Facilities. |
3/04/2009 |
|
1.7 MB |
| Power Considerations for VoIP
Voice over Internet Protocol (VoIP) streamlines business network infrastructures, because one network does the work of two. |
2/15/2009 |
|
183 KB |
| Redefining the economics of running the modern data center
Is your IT organization capitalizing on the latest technology options and best practices? |
2/13/2009 |
|
1.1 MB |
| Parallel UPS configurations
Increasingly, organizations are finding that the risk of running off straight utility power—even briefly—is too great to ignore. So they deploy multiple UPS modules to ensure conditioned power even if one UPS fails. |
1/20/2009 |
|
406 KB |
| Modularity in the data center power infrastructure
Building the data center to meet the needs of an uncertain future is an expensive and needless exercise in over-engineering. New designs need to be modular, with built-in expansion capabilities. |
11/01/2008 |
|
1.2 MB |
| Increase the efficiency of power distribution in your high-density data center
As power density in modern data centers increases, more focus has been placed on improving efficiency in the power distribution infrastructure. |
10/15/2008 |
|
507 KB |
| Considering the effects of UPS operation with leading power factor loads
Over the past five years, a new generation of data processing and communications equipment has become prevalent in modern data centers and network operations centers. |
8/11/2008 |
|
129 KB |
| Is power your weakest link in data center flexibility?
Key considerations for power systems in adaptive IT environments. |
7/15/2008 |
|
51 KB |
| Ten Ways to Protect Your IT Infrastructure
Reduce Costs while protecting critical business systems. |
6/15/2008 |
|
52 KB |
| Distributing Power to Blade Servers
With the growth in blade servers with dual or triple power supplies, a single rack of equipment can easily produce dozens of power cords to manage—and an appetite for 20 kW or more of reliable power. Traditional power strips are just not up to the task. |
5/13/2008 |
|
38 KB |
| Data Center – Unique Characteristics and the Role of Medium Voltage Vacuum Circuit Breakers
Data Centers are a critical part of the world economic systems. Billions of electronic transactions happen via data centers per year. These transactions can contain financial transactions that are critical to the parent company. |
3/13/2008 |
|
1.6 MB |
| High Power UPS Achieves Significant Size and Weight Reductions While Enhancing Performance
First appearing at lower power levels, transformer-free UPS designs have been around two decades or so. |
3/11/2008 |
|
887 KB |
| Electrical Equipment Floor Space: Selected NEC Code Requirements and New Options for the Electrical System Designer
Electrical Equipment Floor Space: Selected NEC Code Requirements and New Options for the Electrical System Designer |
1/16/2008 |
|
373 KB |
| Power factor as it relates to UPS products
This white paper is designed to provide clarification about issues related to UPS power factor (pf). |
1/02/2008 |
|
58 KB |
| Branch Circuit Protection for High Density 208V Power Solutions
The following is an overview of ‘hidden’ issues that some manufacturers are not divulging about the use of Branch Circuit Protection for your high density, mission critical power units. |
11/15/2007 |
|
131 KB |
| Energy efficient transformers reduce data center utility costs
New legislation restricts the type of transformers you can buy, to more expensive models of new design. That’s actually good news for your power distribution system. |
11/14/2007 |
|
74 KB |