White Papers
Eaton's white papers demonstrate how our technology solutions can best address your needs and solve your most pressing business problems.
Title
|
Publication Date | Type | Size |
| Surge Suppression Takes the Bite Out of Transients
An article from the October 2006 Plant Engineering magazine authored by Carey Mossop. |
10/01/2006 |
|
564 KB |
| Straight Talk about Electrolytic Capacitors in your UPS
Electrolytic capacitors are fairly simple devices, ranging in size from a thimble to a soda can, that smooth out fluctuations in electrical voltage. A typical UPS contains a dozen or more different types and sizes of electrolytic capacitors—small ones that smooth out the power supplied to the UPS processor (its on-board intelligence), and large ones to regulate the power that flows to protected equipment. |
3/23/2009 |
|
77 KB |
| Static Auto Tie Mean Time Between Failure Calculations
In a dual power path UPS and distribution system where there are single power cord loads (SPCL) as well as dual power cord loads (DPCL) the availability of protected power to the SPCLs can be greatly increased by the addition of a Powerware® Static Auto Tie (SAT) to the system which will allow the elimination of all the downstream static transfer switches (STS) that serve the SPCLs. |
1/13/2007 |
|
65 KB |
| Right-Sizing Your Power Infrastructure
Data centers today are undergoing unprecedented change, as new technologies such as virtualization, cloud computing help lower operating costs, conserve floor space and simplify management. |
10/26/2009 |
|
597 KB |
| Rethinking Data Center Design
Building the room around the rack can ease cooling challenges and save money |
7/31/2012 |
|
1.1 MB |
| Replacement of hydro plant generator oil circuit breakers with modern vacuum technology
The successful implementation of vacuum generator circuit breakers for this hydro-plant project confirms the practical application and performance of vacuum circuit breakers in the 5000A range. |
9/28/2012 |
|
445 KB |
| Redefining the economics of running the modern data center
Is your IT organization capitalizing on the latest technology options and best practices? |
2/13/2009 |
|
1.1 MB |
| Recommended Installation Practices for CHSPT1 and CHSPT2 Products
UL1449 3rd Edition Surge Products – Eaton Type 1 & 2 Surge Products |
10/17/2012 |
|
64 KB |
| Realizing energy savings in water processing applications using medium voltage adjustable frequency drives
Why uptime and energy efficiency matter in water processing |
8/24/2011 |
|
375 KB |
| Powerware eNotify Remote Monitoring and Diagnostics Service
Eaton offers Powerware eNotify Remote Monitoring & Diagnostics Service for Powerware UPS service contract customers. |
5/13/2007 |
|
1.3 MB |
| Powering Through the Economy
The cost of electricity is already outpacing the cost of hardware. According to The Green Grid, a non-profit organization focused on data centers globally, $1 million worth of servers purchased in 2009 will consume $1.2 million of electricity over a three-year lifespan. Moreover, servers in aggregate account for approximately two percent of US electricity usage. It’s no surprise, then, that for many organizations electrical power now constitutes the largest component of total cost of ownership. |
3/22/2010 |
|
142 KB |
| Power Monitoring 101
Supervisory, connectivity and protection options that add an umbrella of protection over your entire IT infrastructure. |
7/13/2009 |
|
801 KB |
| Power Management for Server Virtualization
Strategies for preserving business continuity and data integrity in virtualized data centers |
4/20/2012 |
|
256 KB |
| Power factor as it relates to UPS products
This white paper is designed to provide clarification about issues related to UPS power factor (pf). |
1/02/2008 |
|
58 KB |
| Power Considerations for VoIP
Voice over Internet Protocol (VoIP) streamlines business network infrastructures, because one network does the work of two. |
2/15/2009 |
|
183 KB |
| Parallel UPS configurations
Increasingly, organizations are finding that the risk of running off straight utility power—even briefly—is too great to ignore. So they deploy multiple UPS modules to ensure conditioned power even if one UPS fails. |
1/20/2009 |
|
406 KB |
| Overcoming Eight Common Power Management Challenges
How intelligent, logical and complete power management solutions provide relief for some of today’s worst power-related headaches. |
2/10/2011 |
|
940 KB |
| Optimizing your Infrastructure for Cloud Computing
This white paper examines some of the forces behind rising adoption of cloud-based solutions, explores how cloud architectures impact data centers and discusses a series of concrete practices and technologies that can help companies collect the benefits of cloud computing without compromising uptime or overwhelming their power and cooling systems. |
8/31/2010 |
|
578 KB |
| Optimizing Power Distribution for High-Density Computing
This white paper shows why 30 amp (30A) three-phase circuits and 30A three-phase PDUs meet the IT demands more efficiently than comparable 20A and 50A alternatives. It also explains why utilizing 30A three-phase circuits and PDUs today puts you in the best position to handle future power capacity needs. |
4/22/2010 |
|
313 KB |
| No Harmony in Harmonics
In this white paper you will read about the trouble with harmonics in modern power systems. Readers will learn about the technical view of harmonics and solutions to compensate for and reduce harmonics. Read the key advantages of HMTs (harmonic-mitigating transformer) and other mitigating techniques. |
2/03/2010 |
|
612 KB |