BECO® MiniCap™ PR Range
Eaton's BECO MiniCaps depth filters are ready-to-use disposable filters for the filtration of small volumes of media containing particles, or for removing micro-biologicals in pharmaceutical and biotechnology applications.
Eaton's BECO MiniCap depth filters have a filter area of 21 cm². With a filtration volume of 1 – 10 liters and suitable for laboratory applications and scale-up trials. Eaton's BECO MiniCap depth filter capsules are available with the BECO PR and PR UltraPure depth filter sheets and used for pharmaceutical and biotechnology applications, or with more open CP2KS types for prefiltration.
Available Options:
BECO MiniCap from the PR UltraPure range
The application of high-purity raw materials such as CELPURE(1) and a special production process ensure minimum content of extractable components (such as aluminum) and minimum endotoxin content (< 0.025 EU/ml). This also results in a 50-percent reduction of the flushing volume to 25 l/m². At the same time, the PR UltraPure series offers approx. 30 % higher throughput compared with conventional depth filter sheets.
BECO MiniCap from the PR range
The PR range was also specially developed for pharmaceutical and biotechnology applications. An innovative production process ensures that the endotoxin content is less than 0.125 EU/ml and offers high endotoxin retention during filtration of different pharmaceutical products.
BECO MiniCap CP2KS
Eaton BECO MiniCap CP2KS depth filter has been optimized for the filtration of strongly colloidal and highly viscous liquids and for liquids containing particles. The high dirt holding capacity enables long service life of the depth filter medium.
Applications
Available Options:
BECO MiniCap from the PR UltraPure range
The application of high-purity raw materials such as CELPURE(1) and a special production process ensure minimum content of extractable components (such as aluminum) and minimum endotoxin content (< 0.025 EU/ml). This also results in a 50-percent reduction of the flushing volume to 25 l/m². At the same time, the PR UltraPure series offers approx. 30 % higher throughput compared with conventional depth filter sheets.
BECO MiniCap from the PR range
The PR range was also specially developed for pharmaceutical and biotechnology applications. An innovative production process ensures that the endotoxin content is less than 0.125 EU/ml and offers high endotoxin retention during filtration of different pharmaceutical products.
BECO MiniCap CP2KS
Eaton BECO MiniCap CP2KS depth filter has been optimized for the filtration of strongly colloidal and highly viscous liquids and for liquids containing particles. The high dirt holding capacity enables long service life of the depth filter medium.
Applications
- Scale-up trials
- Selection of suitable filter media and determination of the required filter area
- Sample preparation
- Separation of cell debris
- Filtration of cell culture media
- Filtration of serum
Loading Content..Please wait!
Thank you for your interest in Eaton's Begerow products. To discuss how our products will meet your specific requirements, please contact your local product specialist listed below. To submit a request for a quote or for additional product information, please use the Contact Us Form.
Current Begerow customers can continue to order from your regular sales representative. For new customers, please refer to the listing below as we develop our new global contact list.
North America - HQ
44 Apple Street
Tinton Falls, NJ 07724
Toll Free: (800) 656-3344
(NORTH AMERICA ONLY)
Voice: (732) 212-4700
China
No. 7, Lane 280, Linhong Road
Changning District, 200335
Shanghai, P.R. China
Voice: +86-21-5200-0099
Singapore
4 Loyang Lane #04-01/02
Singapore 508914
Voice: +65-6825-1668
Brazil
Av. Julia Gaioli, 474-
Bonsucesso
07251-500 - Guarulhos, Brazil
Voice: +55 (11) 2465-8822
44 Apple Street
Tinton Falls, NJ 07724
Toll Free: (800) 656-3344
(NORTH AMERICA ONLY)
Voice: (732) 212-4700
China
No. 7, Lane 280, Linhong Road
Changning District, 200335
Shanghai, P.R. China
Voice: +86-21-5200-0099
Singapore
4 Loyang Lane #04-01/02
Singapore 508914
Voice: +65-6825-1668
Brazil
Av. Julia Gaioli, 474-
Bonsucesso
07251-500 - Guarulhos, Brazil
Voice: +55 (11) 2465-8822
Europe/Africa/Middle East
Auf der Heide 2
53947 Nettersheim, Germany
Voice: +49 2486 809-0
Begerow Product Line
An den Nahewiesen 24
55450 Langenlonsheim, Germany
Voice: +49 6704 204-0
Internormen Product Line
Friedenstraße 41
D-68804 Altussheim, Germany
Voice: +49 6205 2094-0
Auf der Heide 2
53947 Nettersheim, Germany
Voice: +49 2486 809-0
Begerow Product Line
An den Nahewiesen 24
55450 Langenlonsheim, Germany
Voice: +49 6704 204-0
Internormen Product Line
Friedenstraße 41
D-68804 Altussheim, Germany
Voice: +49 6205 2094-0
Products on this site may not be available in all regions. Please contact your local Eaton office to determine availability.