Filters
Fluid Power is one of the most reliable and repeatable forms of power and motion control. When problems are encountered, 80% of the time they are related to inadequate contamination control practices. Eaton has more than a 75-year history of dedication to helping engineers develop, operate and maintain filtration products, as well as cleanliness practices designed to support reliable, high quality power and motion control systems.
Breathers
Hydraulic reservoirs "breathe" air in and out as the oil level rises and falls. This circulating air contains articles and moisture that can cause corrosion, increase equipment wear and reduce fluid performance.
Fluid Analysis
Eaton hydraulic components have a global reputation for quality, reliability and performance. That reputation is built on a tradition of customer service and we stand behind every one of our products. Our Fluid Analysis Service follows that same tradition.
In-Tank Filters
In-tank filters are a special type of low pressure return line filters. In-tank filters are mounted directly to the reservoir tank top and have an accessible head that is located outside of the reservoir while the body of the housing is located inside the reservoir.
Off-Line Filters
Off-line filtration systems (also referred to as a kidney loops or recirculation loops) are typically found in variable volume pump systems where system filters do not see continuous flow or where the return flow volume makes a return filter impractical.
Particle Counter
Eaton’s Target-Pro 2 Portable Particle Counter gives you laboratory quality particle count results in the field. It combines state-of-the-art laser particle counting technology with a user-friendly interface and compact size.
Pressure Filters
Pressure filters are used to protect downstream components from contamination levels beyond the recommended cleanliness target.
Return Line Filters
Return line filters usually have spin-on type elements, cartridge elements in an in-line mounted housing, or cartridge elements within a housing that is mounted directly within the reservoir itself
Spin On Filters
Spin-on filters typically consist of a head mounted directly in-line with the return piping and a canister containing an element which screws onto a threaded post.
Suction Strainers
These Vickers suction strainers protect hydraulic pumps and control systems from solid contaminants.