Low-Speed, High-Torque (LSHT) Motors - Piston

Motors-LSHO Piston category-image


Eaton is proud to be recognized as an industry leader in Low-Speed, High-Torque (LSHT) hydraulic motor technology producing motors that are known for their reliable high-power density, modularity and economic design.

While Power is often defined as the rate of doing work, Torque is defined as the measure of the turning force on an object being rotated, such as a bolt or an automotive flywheel. In the design of mechanical systems, torque density can be used to make smarter design decisions.