Fuller
Fuller manual-shift transmissions are legendary in their solid dependability.
They’re the foundation of the fuel-efficient UltraShift® automated transmissions. Using computer-controlled shifting, Eaton’s automated transmissions are loaded with benefits. The UltraShift transmission improves vehicle safety by making it easier for drivers to keep their eyes on the road and both hands on the wheel.
The latest Eaton automated transmission is the UltraShift PLUS. UltraShift PLUS is stronger, tougher, smarter and more efficient than any other automatic or automated transmission. Available in six models for linehaul and vocational use, each offers maximum power capacity, superior acceleration and low-speed maneuverability.