Vehicle Link Adapters

What You See Is What You Get Element

The following is a list of vehicle link adapters that have been tested with ServiceRanger and are approved for ECU reprogramming.

Manufacturer Product Name
Nexiq USB-Link (Part Number 125032)
Required driver version 9.6.0.2 or greater greater
Nexiq USB-Link 2 Bluetooth (Part Number 124032)
Required driver version 2.3.0.0 or greater
Nexiq USB-Link 2 Wi-Fi (Part Number 124034)
Required driver version 2.3.0.0 or greater
DG Technologies DPA 5 (Part Number DG-DPA5-BT)
Required driver version 2.03 or greater
DG Technologies DPA 4 Plus (Part Number DG-DPA4PLUS)
Required driver version 2.02 or greater
Noregon JPRO DLA+ (Part Number 12206)
Required driver version 4.0.5983.2 or greater
Noregon JPRO DLA+ PLC (P/N 12204)
Required driver version 4.0.5983.2 or greater
Noregon JPRO DLA+ Wireless (P/N 12208)
Required driver version 4.0.5983.2 or greater
Noregon JPRO DLA+ 2.0 (P/N 122061)
Required driver version 4.0.5983.2 or greater
Noregon JPRO DLA+ 2.0 Wireless (P/N 122081)
Required driver version 4.0.5983.2 or greater
Cummins Inline 6 (P/N 2892093)
Required driver version 6.4.1.0 or greater
Cummins Inline 7 (P/N 5299899)
Required driver version 2.3.0.0 or greater

Note: Never use a wireless adapter for ECU programming. Damage to an ECU from using an adapter that has not been approved can result in a void of warranty.


Approved RP1210A Adapters for ServiceRanger 2

The following is a list of approved  RP1210A communication adapters that can be used with ServiceRanger 2:

Manufacturer Product Name
Dearborn Group DPA-II Plus 
Caterpillar CAT Adapter II
Eaton MD-100
(RS-232 connection only, not wireless)
Noregon JPRO Data Link Adapter - Serial port
NEXIQ MagiKey™ Parallel Data Module* (PDM)

Approved RP1202 Adapters for Generation 1 AutoShift Programming

The following is a list of approved communication adapters for Generation 1 AutoShift® programming (RP1202 "pass-thru" adapters)*:

Manufacturer Product Name
Dearborn Group DPA II+
Cummins Inline I, model 3824938
(Windows 95™ only) **
Volvo Adapter, model 9998555
(Windows 95™ only) **
  Generic J1708/RP1202 adapters
(Windows 95™ only) **

Notes:
*Cannot use Serial to USB adapters with RP-1202 communications.
** Intended to be used with the Eaton Serial Communications Driver which is limited to PC’s running Microsoft ® Windows 95™ only.