Filters
Here is a complete line of Filters offerings
Breathers
Hydraulic reservoirs "breathe" air in and out as the oil level rises and falls. This circulating air contains articles and moisture that can cause corrosion, increase equipment wear and reduce fluid performance.
Fluid Analysis
Eaton hydraulic components have a global reputation for quality, reliability and performance. That reputation is built on a tradition of customer service and we stand behind every one of our products. Our Fluid Analysis Service follows that same tradition.
In-Tank Filters
In-tank filters are a special type of low pressure return line filters. In-tank filters are mounted directly to the reservoir tank top and have an accessible head that is located outside of the reservoir while the body of the housing is located inside the reservoir.
Pressure Filters
Pressure filters are used to protect downstream components from contamination levels beyond the recommended cleanliness target.
Return Line Filters
Return line filters usually have spin-on type elements, cartridge elements in an in-line mounted housing, or cartridge elements within a housing that is mounted directly within the reservoir itself.
Spin On Filters
Spin-on filters typically consist of a head mounted directly in-line with the return piping and a canister containing an element which screws onto a threaded post.
Suction Strainers
These Vickers suction strainers protect hydraulic pumps and control systems from solid contaminants.