On-Highway Delivery

On-Highway Truck : Bus

Eaton is the proven innovator in developing products that are more efficient, optimize installation, and reduce total operation costs. Our successful 100-year history is marked with long-term partnerships with major truck, bus, and engine OEMs worldwide.

From the front of the truck to the trailer, Eaton provides fluid and air conveyance solutions for almost every application. Eaton hose styles for transmission oil cooler lines offer peace of mind when using new “green” synthetic oils. Our fuel hose meets today’s engine demands, regardless of engine compartment temperature or fuel type—even 100% biodiesel or compressed natural gas (CNG). And when market demands change in the next three to five years with the introduction of new HFO-1234yf global refrigerant, Eaton will be readily prepared with tested and proven solutions to meet customer needs.