LV DISTRIBUTION TRANSFORMERS
Dry Type Distribution Transformers

The adoption of TP-1 transformer efficiency levels, as part of the EPACT 2005 legislation, has left a void in the area of “next step up” in transformer performance and for those looking to “go green” with their electrical infrastructure. The Eaton E3 (CSL-3 2007 compliant) transformer can fill that void.

The basic purpose of a transformer is voltage transformation as near as practically possible to the load for economy and distribution of power. Typical loads for dry-type distribution transformers include lighting, heating, air conditioners, fans, and machine tools. Such loads are found in commercial, institutional, industrial, and residential structures. Eaton's dry type distribution transformers feature:

  • Frequency - Cutler-Hammer standard dry-type distribution transformers are designed for 60 hertz operation. Transformers required for other frequencies must be specifically designed.
  • Overload Capability - Short term overload capacity is designed into transformers as required by ANSI. Continuous overload capacity is not deliberately designed into a transformer because the design objective is to be within the allowed winding temperature rise with nameplate loading.
  • Seismic Qualified
    The family of Cutler-Hammer dry-type distribution transformers is seismically tested, seismically qualified, and exceeds requirements of the Uniform Building Code (UBC), California Code Title 24 and BOCA.
  • Taps
    Primary taps are available in most ratings to allow compensation for source voltage variations.
  • Series-Multiple Windings
    Series-multiple windings consist of 2 similar coils in each winding which can be connected in series or parallel (multiple). Transformers with series-multiple windings are designated with a “X” or “/” between the voltage ratings, such as voltages of “120/240” or “240 x 480”. If the series-multiple winding is designated by an “X”, the winding can be connected only for a series or parallel. With the “/” designation, a midpoint also becomes available in addition to the series or parallel connection. As an example, a 120 x 240 winding can be connected for either 120 (parallel) OR 240 (series), but a 120/240 winding can be connected for 120 (parallel), or 240 (series), or 240 with a 120 midpoint.
  • Sound Levels
    All transformers make some sound mainly due to the vibration generated in its core by alternating flux. All Cutler-Hammer general purpose dry-type distribution transformers are designed with sound levels lower than NEMA ST-20 maximum levels.

CONFIDENTIAL CONTENT

This section contains information for internal company use only. You can view this content because you are currently connected to the Eaton network. Please do not share this information with people outside of the company.

 
ALL PRODUCTS
1 
2 
3 
DISTRIBUTION PRODUCTS
1 
2 
Learning
Harmonic Mitigating Transformers-Education & Information


Loading Please wait..