Available Logic Control Documents
Click here to search again.

Installation and Activation - Canary Labs Trend Link/Trend Historian
Thefollowing steps must be taken to install and activate your Canary Labs Trend Link and Trend Historian software.Note that that when purchasing a license for the Trend Historian software you also get a license for one copy ofthe Trend Link software. When registering the Trend Link/Trend Historian software you can opt to activate theTrend Link and Trend Historian software on different computers.
IL04804001E.PDF - (PDF, 21KB)

Installation Instructions PanelMate® ePro PS Family Restore Factory Image Load
The restore factory image load kits provide a simple way for users to reset the load of the internal ompactFlash™, which holds the Operating System (OS) to the factory installed image. This gives users a field-recovery method for software problems. The restore factory image load kits are for use with the PanelMate ePro PS models. These include the PanelMate ePro PS, PanelMate ePro PS Classic, PanelMate ePro PS EE (Enterprise Edition), and PanelMate ePro PS OD (Outdoor Series).
IL04801001E.PDF - (PDF, 1MB)

Instructions for Use and Care of the Operator Interface Touchscreen
The Operator Interface is an industrial hardened unit, built to withstand tough environments. Proper use and maintenance of the Operatior Interface will ensure a trouble-free system well beyond the warranty period.
AP04802002E.PDF - (PDF, 100KB)

Modbus+ Network Upload/Download using Windows NT
To get Modbus+ to appear in the port parameters of the Transfer Editor, you must first go to vcpxfer.ini in your Windows NT folder.
AD04804006E.PDF - (PDF, 90KB)

Modbus+ Network Upload/Download using Windows NT
This application note cover includes information and instructions for Easy File Transfers, USB Connectivity, USB DiskOnKey Memory Device.
AD04804003E.PDF - (PDF, 182KB)

PanelMate DeviceNet Communication Driver Manual
This manual describes how to use your operator station with Eaton's Cutler-Hammer DeviceNet PLCs.
MN04803003E.PDF - (PDF, 583KB)

PanelMate ePro Headline Manager - User's Guide
The Headline Manager provides options for alerting operators to events that require attention. The Headline Manager is an application that prominently displays messages on a PanelMate ePro (models XE and SE) Operator Interface unit. These messages appear as headlines in large font, one third screen "pop-up" alert windows on the PanelMate display.
MN04802001E.PDF - (PDF, 604KB)

PanelMate ePro PS and PS EE 15-inch Backlight Replacement Kit - Instructions
This instruction sheet provides a description of how to replace the display backlight in 15-inch PanelMate ePro PS models (7685T-15) and ePro PS EE models (7685T-15E).
IL04805009E.PDF - (PDF, 860KB)

PanelMate ePro PS Data Archiving Registration/Activation - Instructions
The Data Archiving feature must be activated on your PanelMate ePro PS unit before using. A serial number is provided below and is required for registration. The Data Archiving feature is configured using ePro Canvas Professional (Version 2.20 or above) and it can be tested on an inactivated ePro PS unit and on your PC for up to 60 minutes at a time.
IL04805007E.PDF - (PDF, 32KB)

PanelMate ePro PS Family - Users Guide
Comprehensive users guide for the PanelMate ePro PS family including information on initial power up, connectivity, software/file loading, run mode, and hardware installation requirements. Cutout and dimensional diagrams are included. Information included for PanelMate ePro PS, OD, EE and Classic models.
MN04802013E.PDF - (PDF, 1MB)

PanelMate ePro PS PCI Adapter - Instructions
Instructions for installing the PCI adapter on a PanelMate ePro PS 12", 15", and Blind Node models.
IL04805001E.PDF - (PDF, 161KB)

PanelMate ePro PS Recipe Management Registration/Activation - Instructions
The Recipe Management feature must be activated on your PanelMate ePro PS unit before using. A serial number is provided below and is required for registration. The Recipe Management feature is configured using ePro Canvas Professional (Version 2.20 or above) and it can be tested on an inactivated ePro PS unit and on your PC for up to 60 minutes at a time.
IL04805008E.PDF - (PDF, 32KB)

PanelMate ePro PS Series 12-inch Backlight Replacement Kit - Instructions
This instruction sheet provides a description of how to replace the display backlight in 12-inch PanelMate ePro PS models (7685T-12), ePro PS EE models (7685T-12E), and ePro PS OD models (7685T-12OD)
IL04805011E.PDF - (PDF, 1MB)

PanelMate PC DDE Connectivity Communication Driver Manual
This Manual tells how to use your PanelMate PC operator station to retrieve and receive information from other Microsoft Windows programs via a DDE (Dynamic Data Exchange) conversation.
MN04803002E.PDF - (PDF, 570KB)

PanelMate Power Pro 1785x, ePro 7585x-8 and ePro PS 7685x-8 Backlight Replacement Kit - Instructions
This instruction sheet provides a description of how to replace the display backlight in 8-inch TFT displays used in the PanelMate Power Pro 1785x models, PanelMate ePro 7585x-8 models and PanelMate ePro PS 7685x-8 models.
IL04805010E.PDF - (PDF, 1MB)

PanelMate Power Pro Adapter Mounting Kit - Instructions
Installation instructions for the Adapter Mounting Kit which permits mounting aPanelMate Power Pro 1700 TouchPanel unit in alocation previously occupied by a PanelMate PowerSeries 2000 (model 24xx) TouchPanel unit. TheAdapter Collar is approved for use in Type 12installations when properly mounted in acorrespondingly rated enclosure.
150487.PDF - (PDF, 80KB)

PanelMate Power Pro Configuration Editor Software User's Guide
This manual provides information on installation, use and features of the PanelMate. Power Pro Configuration Editor.
MN04803016E.PDF - (PDF, 3MB)

PanelMate Power Series Mitsubishi Communication Driver Manual
This manual describes how to use the Operator Station with Mitsubishi PLCs. The manual is organized into: Possible Configurations, Cabling, Communication Parameters, Mitsubishi Word and Bit References, and Maintneance Access.
MN04803005E.PDF - (PDF, 1MB)

PanelMate Power Series Modbus Plus Interface Board Installation
Instructions for installing a Modbus Plus Communications Interface Board (Cat # 0748-1, 0748-2) in a PanelMate Power Series unit. The Modbus Plus Communication Interface allows the PanelMate unit to communicate on a Modbus Plus network.
150463.PDF - (PDF, 230KB)

PanelMate Power Series Omron Communication Driver Manual
This manual describes how to use the Operator Station with Omron PLCs. The manual is organized into: Possible Configurations, Cabling, Communications Parameters, Word and Bit References, and Maintenance Access.
MN04803007E.PDF - (PDF, 569KB)

PanelMate Power Series PLC Direct Communication Driver Manual
This manual describes how to use the Operator Station with PLC Direct PLCs. The manual is organized into: Possible Configurations, Cabling, Communication Parameters, Word and Bit References, and Maintenance Access.
MN04803008E.PDF - (PDF, 578KB)

PanelMate Power Series ROBOX Communication Driver Manual
This Manual describes how to use the Operator Station with a ROBOX 486 industrial computer. The manual is organized into: Possible Configurations, Cabling, Communication Parameters, Word and Bit References, and Maintenance Access.
MN04803011E.PDF - (PDF, 332KB)

PanelMate Power Series Siemens Communication Driver Manual
This Manual describes how to use the Operator Station with Siemens PLCs. The manual is organized into: Possible Configurations, Cabling and Communications Parameters, Word, Byte, and Bit References, and Maintneance Access sections.
MN04803012E.PDF - (PDF, 1MB)

PanelMate Power Series Square-D Communication Driver Manual
This manual describes how to use the Operator station wit Square D PLCs. The manual is organized into: Possible Configurations, Cabling, Communication Parameters, Word and Bit References, and Maintenance sections.
MN04803013E.PDF - (PDF, 499KB)

PanelMate Power Series Texas Instruments Communication Driver Manual
This Manual describes how to use the Operator Station with Texas Instruments PLCs. The manual is organized into: Possible Configurations, Cabling, Communication Parameters, Word and Bit References, and Maintenance Access sections.
MN04803014E.PDF - (PDF, 822KB)

PanelMate reg; ePro - Users Guide
Comprehensive users guide for the PanelMate ePro including information on initial power up, connectivity, software/file loading, run mode, troubleshooting and hardware installation requirements. Cutout and dimensional diagrams are included.
PU04802002E.PDF - (PDF, 2MB)

PanelMate® ePro PS Family User Manual
The PanelMate ePro PS family is made up of high performance yet cost-effective operator interface (OI) products. The ePro PS family carries on the PanelMate tradition of performance in balance with ease of use.
MN04801001E.PDF - (PDF, 2MB)

Replacing Micro PanelMate D820, D830, or D840 with ELC-GP04
This Adapter Plate Kit (APPM1ELCGP4) allows you to mount an ELC-GP04 unit in a location previously occupied by a Micro PanelMate D820, D830, or D840 unit.
Pub51983.PDF - (PDF, 43KB)

Replacing PanelMate 3000 or 10” ePro Keypad unit with a 10” PanelMate® ePro PS or PanelMate 3000 Touch Screen unit
This Adapter Plate Kit (APPS10A) allows you to mount a PanelMate ePro 10” display unit (7685T-10 series) or a PanelMate 3000 display unit (3985T-10 series) in a location previously occupied by a PanelMate 3000 Keypad (3985K series) or a 10” PanelMate ePro Keypad unit (7585K-10 series).
pub51978.pdf - (PDF, 32KB)

Replacing PanelMate 3000 Touchscreen Display with an HMI10CE
This Adapter Plate Kit (APPS12B) allows you to mount a PanelMate 12” ePro ePro PS touch screen unit in a location previously occupied by a PanelMate Power Pro 5000 Keypad unit.
Pub51986.PDF - (PDF, 34KB)

Replacing PanelMate Keypad with an HMI08CE
This Adapter Plate Kit (APPM1HMI8) allows you to mount an 8” HMi unit in a location previously occupied by a PanelMate 1100 or 1700 keypad unit.
Pub51984.PDF - (PDF, 34KB)

Replacing PanelMate Touch Panel and Keypad with PanelMate Touchscreen
This Adapter Plate Kit (APPS8A) allows you to mount a PanelMate 1100, 1700, 8” ePro, or 8” ePro PS touch screen unit in a location previously occupied by a PanelMate 1100, 1700, 8” ePro Keypad unit.
Pub51987.PDF - (PDF, 34KB)

Replacing PanelMate Touch Panel and Keypad with PanelMate Touchscreen
This Adapter Plate Kit (APPS12B) allows you to mount a PanelMate 12” ePro ePro PS touch screen unit in a location previously occupied by a PanelMate Power Pro 5000 Keypad unit.
Pub51988.PDF - (PDF, 34KB)

Replacing PanelMate Touchscreen Display with an HMI10CE
This Adapter Plate Kit (APPM1HMI10) allows you to mount a 10” HMi unit in a location previously occupied by a PanelMate 3000 touchscreen display.
Pub51985.PDF - (PDF, 34KB)

Replacing the PanelMate ePro PS, PanelMate ePro PS Classic, and PanelMate ePro PS EE 7685x-10x Series
The Backlight Replacement Kit provides a replacement backlight for the PanelMate ePro PS 7685T-10 Series, the PanelMate ePro PS Classic 7685T-10C Series, and the PanelMate ePro PS EE (Enterprise Edition) 7685T-10E. Although the figures provided are for the ePro PS models, the disassembly for the ePro PS Classic and ePro PS EE models are the same.
IL04802007E.PDF - (PDF, 630KB)

Replacing the PanelMate ePro PS, PanelMate ePro PS Classic, PanelMate ePro PS EE, and PanelMate ePro PS OD 7685x-12 Series Backlight Assembly
The Backlight Replacement Kit provides a replacement backlight for the PanelMate ePro PS 7685T-12 Series, the PanelMate ePro PS Classic 7685T-12C Series, the PanelMate ePro PS EE (Enterprise Edition) 7685T-12E Series, and the PanelMate ePro PS OD (Outdoor) 7685T-12OD Series. Although the figures provided are for the ePro OD models, the disassembly for the ePro PS, Classic and ePro EE models are the same.
IL04802006E.PDF - (PDF, 637KB)

Replacing the PanelMate ePro PS, PanelMate ePro PS Classic, PanelMate ePro PS EE, and PanelMate ePro PS OD
The Backlight Replacement Kit provides a replacement backlight for the PanelMate ePro PS 7685T-15 Series, the PanelMate ePro PS Classic 7685T-15C Series, the PanelMate ePro PS EE (Enterprise Edition) 7685T-15E Series, and the PanelMate ePro PS OD (Outdoor Series) 7685T-15OD. Although the figures provided are for the ePro PS models, the disassembly for the ePro PS Classic, ePro PS EE and ePro PS OD models are the same.
IL04802009E.PDF - (PDF, 575KB)

Replacing the PanelMate® ePro PS and PanelMate ePro PS EE 7685x-15 Series Backlight Assembly

01-50606.pdf - (PDF, 865KB)

Using the Email Action in Canvas Software for Remote Notification
The Email Action in Canvas software can be used for a variety of remote notification applications. Coupled with open source desktop sharing tools for remote access to an ePro PS, the Email action completes a set of remote notification and debugging tools.
AP04801005E.PDF - (PDF, 99KB)