To accurately calculate the pressure loss for filters and strainers in a pipeline, proceed as follows:
- First calculate pressure loss using Cv factor formula at right
- Take the pressure loss figure obtained in (1) and recalculate it using the appropriate correction factor from the following tables.

The pressure loss across a strainer or filter can be calculated using the system's flow rate and the Cv factor for that strainer or filter.
For example, a 1 " strainer with a Cv factor of 8 will have a 4 psi pressure loss in a system with a 16 gpm flow rate: (16 ÷ 8) 2 = 4.
If you would like us to contact you regarding an application or product, please
click here.
Water Only
Multiply the pressure drop for perforated baskets by the following.
|
|
| 40 Mesh |
1.2 |
| 60 Mesh |
1.4 |
| 80 Mesh |
1.6 |
| 100 Mesh |
1.7 |
| 200 Mesh |
2.0 |
| 325 Mesh |
2.5 |
|
| First-Multiply the pressure drop for water shown in charts by the specific gravity of the liquid. Second-Multiply the corrected pressure drop figure by the following correction factors for more viscous liquids. (Water has a viscosity of 30 SSU.) |
|
|
|
|
|
|
|
|
| 500 |
1.6 |
1.9 |
2.1 |
2.4 |
2.6 |
3.1 |
3.6 |
| 1000 |
1.7 |
2.2 |
2.4 |
2.6 |
2.8 |
3.3 |
3.8 |
| 2000 |
1.9 |
2.4 |
2.7 |
2.9 |
3.2 |
3.8 |
4.0 |
| 3000 |
2.0 |
2.6 |
2.9 |
3.2 |
3.5 |
4.1 |
4.3 |
| 5000 |
2.2 |
3.0 |
3.5 |
4.0 |
4.5 |
5.3 |
6.3 |
| 10000 |
2.5 |
3.5 |
4.2 |
5.0 |
6.0 |
7.1 |
8.5 |
|
|
|
|
|
| 400 |
0.0015 |
0.0381 |
38 |
| 300 |
0.0018 |
0.0457 |
45 |
| 250 |
0.0024 |
0.0609 |
60 |
| 200 |
0.0027 |
0.0686 |
68 |
| 150 |
0.0041 |
0.1041 |
104 |
| 100 |
0.0065 |
0.1651 |
165 |
| 80 |
0.007 |
0.1778 |
177 |
| 60 |
0.009 |
0.2286 |
228 |
| 40 |
0.015 |
0.380 |
380 |
| 20 |
0.034 |
0.8636 |
862 |
|
|
|
|
|
| 1/32 |
0.033 |
0.838 |
838 |
| 3/64 |
0.045 |
1.143 |
1143 |
| 1/16 |
0.070 |
1.778 |
1776 |
| 3/32 |
0.094 |
2.387 |
2387 |
| 1/8 |
0.125 |
3.175 |
3175 |
| 5/32 |
0.150 |
3.810 |
3810 |
| 3/16 |
0.1875 |
4.762 |
4762 |
| 1/4 |
0.250 |
6.350 |
6350 |
| 3/8 |
0.375 |
9.525 |
9525 |
| 1/2 |
0.500 |
12.700 |
12700 |
|