Electrical United States | Worldwide Sites | eaton.com   
 
EDUCATIONAL FACILITIES

universityOften, educational facilities have aging infrastructures. Many campus power systems were built over several decades, resulting in a collection of equipment varying in age and manufacturer that is difficult to manage and maintain. Eaton's solutions including measurement and verification, helps educational facilities take control of their power systems; cutting costs and meeting the modern expectations of on-campus technology.

 
Products and Services
1 
2 

College and University Facility Managers typically spend between 35% and 50% of their operating budgets on energy, and this cost is increasing. It is becoming widely accepted that the functionality of traditional building management systems does not lend itself to providing the necessary tools required to manage power quality, reliability and energy.

Eaton’s measurement and verification solutions will help you monitor and measure your power and energy usage, providing actionable information to help you save costs.

  • Easily justifiable cost with built-in payback; the costs of a measurement and verification system can be justified by the savings realized by taking action on actual energy usage information
  • Full line of metering solutions to fit your differing needs
    • Easy installation due to a limited number of footprints, similar wiring, and retrofit capabilities
    • Will fit into your existing building management systems; vendor neutral, open architecture / protocol communications
    • No software necessary; view information from a standard internet browser and IP address
  • Establish Baselines to find areas to reduce energy, GHG Emissions and build an energy conscious culture
  • Opportunities to increase revenues through sub metering; providing an energy bill for special events, building billing/cost allocations, load profiles to identify equipment problems
  • Participate in available Demand Response programs; system can display sheddable loads, the current consumption of those loads allowing you to shed the necessary consumption


Additional Information:

  • Eaton's solutions enable an institution to manage the power system as a single, integrated system, but more importantly, they help bring a facility's current infrastructure up to today's standards. Eaton's EESS team can evaluate the overall electrical system and implement solutions in educational facilities that help save money and avoid service interruption.
  • UPS units ensure clean, uninterrupted power to keep critical functions running until backup generators take over. If power fails, no data is lost.
  • Eaton can help educational facilities manage energy costs proactively with solutions to help address the pressures of reducing greenhouse gas emissions and overall energy costs.
  • Power Xpert meters and software track energy usage across the entire campus to find opportunities for savings, while Eaton's performance-based approach to maintenance reduces costs by extending equipment life and avoiding emergency repairs.
  • Because keeping people safe is of the utmost importance, Eaton's products are designed to distance people and equipment from hazards.
  • Eaton is a leader in arc flash prevention technologies. In addition, Eaton offers comprehensive scalable diagnostic studies that help identify potentially catastrophic risks and training for employees to help them spot and avoid dangers like electrical shock.

Systems analysis and designSystems analysis and design
Eaton engineers create a comprehensive view of the entire power system. With that information, flexibility is strategically built into the system, so that the power system can adapt to changing requirements.

Energy auditsEnergy audits
Eaton engineers identify wasteful patterns in total energy consumption from all sources—electricity, steam, gas and compressed air—and recommend more efficient solutions to reduce overall energy use.

trainingTraining
Eaton offers training for employees to teach them how to spot danger and avoid it. With this knowledge, employees can do a better job of protecting themselves.

Project managementProject management
Eaton project managers offer a single point of accountability for complex construction projects. This streamlines coordination, helping complete projects on time and on budget with turnkey assistance.

Satellites and Services CentersSatellites and Services Centers
Eaton is the only electrical manufacturer with regionally located manufacturing plants across the United States to cater to your individual needs. Satellites can specify, develop and manufacture customized products and solutions locally. This gives customers local access to market knowledge and in-depth technical skills and lets them take advantage of emergency response and quick-ship schedules when required.

Arc flash hazard analysisArc flash hazard analysis
This service identifies places in the power system where there is risk of an arc flash event. Once dangers are known, they can be managed with equipment, training and proper labeling.

Paralleling switchgearParalleling switchgear
If power is interrupted, the paralleling switchgear manages critical transactions from the power company to an onsite generator, protecting vital health care functions from any disruption.

Protective and predictive relaysProtective and predictive relays
When there is a surge in power, protective relays help to isolate the problem and protect the rest of the system from failing. Predictive relays continuously monitor insulation on circuits and alert workers of potential failures.

Quick connectQuick connect assembly
These assemblies allow connecting a generator to be done quickly and easily without requiring the help of skilled electricians.

UPS unitsUPS units
If utility power fails, UPS units ensure clean, uninterrupted power to keep critical functions up and running until backup generators take over.

Power Xpert software and metersPower Xpert software and meters
Monitor the power system in real time using Power Xpert meters and software. Information about system performance allows managers to troubleshoot problems before they happen.

Variable frequency drivesVariable frequency drives
These drives adjust a motor’s speed to match changing output requirements, conserving energy and allowing the system to be more responsive.

Power factor correction capacitorsCapacitors
Reduce consumption by generating the reactive power needed to improve power utilization with capacitors (instead of sourcing it from the utility), and save on energy costs immediately.

Harmonic mitigating transformersHarmonic mitigating transformers
Harmonic mitigating transformers reduce harmful harmonic currents that disrupt the flow of useful energy in a circuit. Fewer harmonics makes energy consumption more efficient, thus reducing overall energy consumption and lowering energy costs.

Lighting control software and occupancy sensorsLighting control software and occupancy sensors
When a room is empty, the lighting control software turns off the lights. Lighting control software also reduces artificial lighting when the natural light is strong, reducing overall energy consumption and costs.

Circuit breakers and ground fault circuit interruptersCircuit breakers and ground fault circuit interrupters (GFCIs)
GFCIs shut down a circuit when the device detects a leak of current, protecting people from electric shock.

Arcflash Reduction Maintenance System and remote power rackingArcflash Reduction Maintenance System and remote power racking
These solutions protect workers by reducing the duration of arc flash events and increasing the distance between workers and electrical currents during maintenance.

Surge protection equipmentSurge protection equipment
The protection devices detect anomalies and temporarily divert surge current away from the equipment, eliminating damage to the power system.

Arc fault circuit interrupters (AFCIs)Arc fault circuit interrupters (AFCIs)
These devices detect dangerous arcs in the power flow. When the interrupter detects an arc, it stops the flow of current through the circuit, reducing the risk of fire.

Alternative energyAlternative energy
Eaton is an industry leader in providing alternative energy solutions, including solar and wind installations and electric vehicle, hybrid-electric vehicle and electric vehicle charging.

Electric vehicleElectric vehicle
Eaton is an industry leader in electric vehicle (EV) and hybrid electric vehicle (HEV) components, including systems that provide fuel savings ranging from 30 to 60 percent. In addition, Eaton now provides the most robust, flexible offering of electric vehicle supply equipment (EVSE) on the market. Eaton’s Pow-R-Station family of solutions is the electric transportation industry’s premier EVSE.

Integrated facility system (IFS)Integrated facility system (IFS)
Eaton's IFS solutions are designed to shorten your construction time with prefabricated transformers, switchboards, UPSs, lighting control and DC power units. Because the equipment is ready to install and designed to save space, you save on construction costs.

Loading Please wait..