![]() |
|||||
|
|
Loading Please wait..Green Power Equipment Solutions for the Forest Products Industry +/-
While major manufacturers are partnering with universities and engineering firms to make this technology practical, individual lumber and pulp and paper mills are being made greener and more energy-efficient with Eaton products and system design expertise. For instance, a pulp and paper mill built in the 1960s by a major forest product company in the northwestern U.S. was recently able to forestall the building of an entire substation thanks to a new power management system from Eaton. The system, which encompassed a comprehensive and coordinated array of Power Xpert metering and protective devices, monitoring and communications equipment, and software, identified several areas in the plant’s electrical distribution that had been over-designed and could handle additional power capacity. Because the new power management system also served to facilitate more efficient distribution of the mill’s power load, plans to add a new and expensive substation were scrapped. In addition to these cost savings, the new system yielded a long list of other energy- and cost-saving benefits, including improved system reliability, the implementation of a predictive maintenance program, the ability to negotiate for better electrical rates, and more. Predictive Maintenance Solutions +/-
With the cost of downtime in a large integrated pulp and paper mill ringing in at over $50,000/hour, historic methods to prevent downtime involve time based preventive maintenance practices or scheduled outages. Although this method of maintenance is available at a lower cost than downtime, it is still very expensive and often times ineffective. Preventive maintenance is invasive by design and can sometimes end up being the cause of premature equipment failure. Over 40% of the time that a needed part is identified during a scheduled outage, it is found to not be readily available. The Forest Products Industry is quickly moving toward predictive diagnostic methods. This approach assures that uptime is maximized at the lowest possible cost. Because this approach is non-invasive in nature, the plant can continue to run efficiently while critical components of the system are being checked for reliability and integrity. Facility electrical maintenance is able to diagnose potential problems in advance, while minimizing exposure to potential arc-flash hazards typically encountered during scheduled outages. Eaton offers leading technology solutions to drive today's industry toward a more efficient and cost effective predictive maintenance model. Installations of Motor Control Centers have changed the tools used by our customer's maintenance electricians from a volt-ohm meter to an operator interface control station. Predictive Diagnostics products such as the Insulgard partial discharge monitoring system have led the way in predicting future failures in large motors, generators and medium voltage switchgear well before the failures actually occurred. Be sure to read how the Forest Products Industry is working together with Eaton to drive toward this lower cost maintenance model. Generator Life Cycle Extension Solutions +/-
Today most integrated pulp and paper mills own and operate at least one steam-turbine generator, typically rated from 10 to 80 Megawatts. Several of the industry's existing generator assets were built in the '50's and '60's and are beginning to show their age. Eaton has demonstrated industry leadership as a total solutions provider in upgrading existing generator systems at paper mills. Four areas where Eaton's Electrical Engineering Services offers solutions include:
As on-site power generation systems become more important to integrated paper mills, Eaton offers leading solutions to assure reliable, low cost operation. With over 100 years of industry experience, we understand power generation systems and have the answers to assure your existing generation assets are running efficiently. |
||||