Electrical United States | Worldwide Sites | eaton.com   
 
MCC AFTERMARKET SOLUTIONS
MCC AftermarketEaton supports every vintage of MCC ever produced under the brand names of Eaton, Cutler-Hammer and Westinghouse. In addition, Eaton provides aftermarket solutions for the following manufacturers’ units: Moeller, Allen-Bradley, General Electric, ITE/Gould, Siemens/Furnas, Square D, and FPE. Our product line offers overnight replacements from eight locations. Standard lead times vary from 1-4 weeks. Contact us today for your MCC Aftermarket opportunity!
 
Products and Services
1 
2 

Eaton’s MCC aftermarket units offer many standard features to ensure customers that the product they receive is new and genuine from the factory. Included are factory seals, inspection stickers, date codes and a UL 845 label.

  • Brand new unit includes new unit wrapper with new stab assembly, new components, and net door and mounting hardware.
  • Units can be built per custom wiring diagrams for reduced time and ease of installation.
  • Modernization options are available such as soft starters, variable frequency drives, metering and communications.
  • Arc flash safety options are available by replacing existing Freedom 2100, IT., Advantage, and Series 2100/5 Star units with Eaton’s FlashGard units.
  • Units available in as fast as one day!
  • Eaton offers 8 manufacturing plants to build units for you!
Call Us IconCall us: 1-800-653-8648
Locate a Service Center

Loading Please wait..

Vintage Cutler-Hammer FAQs
9800 Unitrol | F10 Unitrol | Freedom Unitrol
These models are identified with serial numbers.

No, vintage Cutler-Hammer motor control centers used serial numbers in lieu of general order numbers for tracking.
There is no specific location the serial number can be found. The serial numbers can be found in the horizontal or vertical wire way doors. As well as on back pans or individual unit doors.
There is no specific location the serial number can be found. The serial numbers can be found in the horizontal or vertical wire way doors. As well as on back pans or individual unit doors.
6AF45XXXX through 6AF62XXXX. (All serial numbers should be verified for vintage prior to order entry)
6AF78XXXX through 6AF119XXXX (All serial numbers should be verified for vintage prior to order entry)
6AF12XXXXX and above e.g. 6AF13XXXXX, 6AF14XXXXX, etc. (All serial numbers should be verified for vintage prior to order entry)
All 6CF, 6LF, 6PF, and 6HF will either be F10 Unitrol or 9800 Unitrol. No specifics on the serial numbers for at glance identification
Yes, it is possible to identify vintage without the general order number or serial number by using original unit class types usually found on original MCC documentation.
9818 = FVNR w/breaker
9828 = FVR w/breaker
9824 = FVNR w/fusible disconnect
9814 = FVR w/fusible disconnect
9808 = Feeder w/breaker
9804 = Feeder w/fusible disconnect
F40 = FVNR w/breaker
F80 = FVR w/breaker 
F30 = FVNR w/fusible disconnect 
F70 = FVR w/fusible disconnect 
F60 = Separate winding w/breaker 
F50 = Separate winding w/fusible disconnect 
F65 = Reconnectable w/breaker 
F55 = Reconnectable w/fusible disconnect 
F91 = Feeder w/Breaker 
F90 = Feeder w/fusible disconnect 
F96 = Dual Feeder w/fusible disconnect 
F97 = Dual Feeder w/breaker
VN24 = FVNR w/breaker 
VN28 = FVR w/breaker 
VN54 = FVNR w/fusible disconnect 
VN58 = FVR w/fusible disconnect 
VN37 = Separate winding w/breaker 
VN67 = Separate winding w/fusible disconnect 
VN29 = Reconnectable w/breaker 
VN59 = Reconnectable w/fusible disconnect 
VN21 = Feeder w/Breaker 
VN51 = Feeder w/fusible disconnect 
VN52 = Dual Feeder w/fusible disconnect 
VN22 = Dual Feeder w/breaker

Cutler-Hammer | Vintage Westinghouse FAQs
These models are identified with general order number.

A general order number is generated once a purchase order is entered on the Vista system. The Vista system is a global system used by Eaton to track ship dates, products, orders entered and sales billed.
The general order numbers for the Freedom, Advantage, and Series 2100 motor control centers will be found externally on the horizontal wire way door. The general order number and unit numbers are also located on labels within the units. The unit labels are typically located on the right wrapper side.
The general order numbers for Vintage Westinghouse are located in the first or second structure of the line up. The numbers are inside the horizontal or vertical wire way doors.
Typical general order numbers have as few as two (2) and as many as four (4) characters beginning in the number and then 4-5 digits preceding the characters. The general order number will also have an item number. Provide the general order number and item number when requesting quotations. There were also general order numbers that were all digits. Typically, this indicated a distributor entered the order direct.
HUPG10332 item 001, HUIN10151item 1, AT51070 item 56, TLI63704 item 010, & 336519225 item 001
Call Us IconCall us: 1-800-653-8648
Locate a Service Center