Got a Power Xpert Meter 4000 and need more detailed features to monitor your power quality? Unleash the full potential of your power quality meter TODAY!
Do more with what you have with the click of the mouse! You can now transform your existing Power Xpert Meter 4000 into the Power Xpert Meter 6000 that offers close to a dozen enhanced features to help you extend equipment life, prevent downtime, and more..
You may be thinking, “This sounds good, but what exactly are the benefits to me?”
Good question. To help answer this we’ve put together the table below to show you the features and benefits you will realize from a 6000 meter vs. a 4000 meter. Click on each new feature for a more detailed explanation and its benefit to you. After reviewing this information we’re sure you’ll agree that this upgrade is a must have for those expected to do more with what you have.
Feature
Power Xpert Meter 4000
Power Xpert 4000 w/Upgrade (PXM6000)
Event logging
•
•
Standard Memory**
2 GB
2 GB
Delta-Sigma D/A Conversion Technology
•
•
Harmonics over-sampling (4096 samples per cycle)
•
•
Anti-Alias Filtering
•
•
Sub-cycle disturbance capturing
•
•
dV/dt triggers for sub-cycle oscillatory transients
*Please note that a first generation Power Xpert Meter 4000 can only be upgraded to a first generation Power Xpert Meter 6000. A second generation Power Xpert Meter 4000 can be upgraded to a second generation Power Xpert Meter 6000. Once and upgrade is purchased, you will be sent the appropriate key for upgrade based on your serial number. **When upgrading online, the memory capacity remains at 2 GB.
NOTE: These specifications are subject to change without notice and represent the maximum capabilities of the product with all options installed. This is not a complete feature list. Features and functionality may vary depending on selected options, product model and firmware version. Please refer to the technical data sheet and User Manual for detailed specifications.
Power Xpert Meters each provide unique additional functions.
The Power Xpert Meter 4000 Provides all the core functions for monitoring power consumption and power quality. This unit uses Delta Sigma technology to oversample circuits at 4096 samples per cycle for extremely accurate measurement of harmonics, power factor, energy consumption, low frequency transient detection/capture and other events.
The Power Xpert Meter 6000 This meter provides all the capabilities of the Power Xpert Meter 4000 plus enhanced power quality monitoring with automatic, industry standard trigger settings and plots events on an ITIC (Information Technology Industry Council) performance curve so they can be easily analyzed. Also provides an Events Calendar view for instant insight to the frequency of power events and helps detect reoccurring problems. View and understand the sequence of events that have occurred during a period of time by selecting on one of the dates in the Events Calendar.
Power Xpert Meter 4000/6000 Series Features:
Embedded Web Server-see and analyze waveforms, trends, harmonics directly in your web browser or LCD meter graphic display
Automatic power quality analysis and trigger setting with built-in ITIC performance curve: detect and capture sags, swells, and flicker
Comprehensive power, energy and demand measurements for 138 standard data points logged
Up to one millisecond time synchronization and event logging capability for sequence of events analysis
Get an at-a-glance view of power quality with patent-pending Power Quality Index gauge, statistically derived trending and red/yellow/green indicators for overall power health
Alarm notifications are also available remotely via e-mail with waveform attached
ANSI C12.20 accuracy
How to upgrade? Upgrading an existing Power Xpert Meter 4000 to a Power Xpert Meter 6000 is simple and easy. Start by clicking the “Buy Now” button below and follow the instructions. Please make sure that you have the following handy and available: your credit card, your Power Xpert Meter 4000 serial number and date code (you will be presented with this info if you are using the upgrade link directly from your Power Xpert Meter) and your e-mail address.
Once you have completed the purchase, we will send you your new license key information via email that will allow you to complete the upgrade.
Enhanced Power Quality Index
The patent-pending Power Quality Index gives a quick visual on the ‘temperature’ of your power quality. If the gage shows in the yellow or red, you’ll know immediately there is an issue that needs attention. The gauges alarm levels are based on current TDD%, voltage THD%, K and C factors, flicker and ITIC events measurements. With the enhanced power quality index, you will be able to see more detailed information when selecting the latest 10 minute and latest 24 hour links.
Can also detect and quantify low frequency RMS voltage variations causing incandescent lighting flicker. This helps determine if the thresholds of the flicker calculation are within your assigned parameters to identify voltage variations.
Interharmonics
Allows you to see the effects of loads that are not multiples of 60 HZ such as variable speed drives. Once the harmonics are identified, you will be able to address with harmonic mitigation.
Enhanced ITIC Curve Plots with automatic trigger settings and event severity counters
The ITIC (Information Technology Industry Council) curve describes how much (or how little) voltage your IT equipment can sustain without damage, over what length of time. When you can plot power events in this broader context — relative to multiple variables — you can identify trouble that could cause damage or may be brewing.
The ITIC performance curve comes prepopulated with sag, swell, and transient triggers to get you up and running immediately on identifying power anomalies. The ITIC Web page also includes counters to track the occurrence of disturbances and a pass/fail summary. In addition, selecting any disturbance counter links to a detailed event view of the disturbances in that ITIC category. The enhanced ITIC curve is also color coded for quick identification of power problems. Disturbance waveforms can be viewed from the browser.
Event Calendar View
The Event Calendar view provides instant insight to the frequency of power events and helps detect reoccurring problems. Color-coded events can be filtered to detect specific issues.
Events Timeline View with sequence of events and events plot on waveform
By selecting on one of the dates in the Events Calendar, you can view and understand the sequence of events that have occurred during a period of time. Plot color-coded events on a captured waveform to gain insight into the sequence of events from one single cycle to the next one. This provides the user an excellent vantage point to review and compare multiple events at an unprecedented resolution.