Eaton’s phase-balanced meter stack uses fewer stacks for complete phase balancing. As electrical rooms grow smaller, the need is greater than ever to provide space-saving metering products as part of a fully phase-balanced system. Eaton's phase-balanced stack is the answer. The new phase balanced stacks connect the two bottom meters to phases B and C and the top two or three meters to phases A and C. Using these new stacks with the AB phased 3MM metering, phase balancing is accomplished.