New Brochure Highlights Spicer® Heavy-Duty Tandem Drive Axles
KALAMAZOO, Mich. … A new six-page brochure from Dana Corporation’s Commercial Vehicle Systems group highlights the features and benefits of the Spicer® D170 and D190 series of heavy-duty, single-reduction tandem drive axles. The brochure and ordering information are available at http://www.roadranger.com/heavytandems.
The brochure emphasizes the robust design features of the Spicer D170 and D190 axles by providing side-by-side comparisons with competitive axle designs. These features include wider faced hypoid gearing for greater strength, integrated systems design with 50 percent fewer parts than competitive designs for enhanced reliability, and a unitized ring gear bolting system with 20-millimeter bolts for maximum joint retention.
The brochure also describes the heavy-duty axle series’ larger tapered bearing systems; larger wheel differential gearing; and stronger, heat-treated steel differential cases – which result in enhanced performance, strength, durability, and reliability.
The brochure also includes information on several patented technologies that are used in the manufacturing of Spicer heavy-duty tandem axles. These include patented differential bearings that ensure precise bearing adjustments, patented on-demand lube pumps that lower operating temperatures and reduce fuel consumption, a patented driver-controlled differential lock option that promotes maximum traction, and patent-pending threaded input cages that eliminate leak paths and improve bearing adjustment.
Spicer D170 series heavy-duty tandem axles, with a broad ratio coverage of 3.07 to 7.17:1, are available for applications with gross axle weight ratings of 40,000, 46,000 and 50,000 pounds. Spicer D190 series heavy-duty tandem axles, with ratio coverage of 3.42 to 7.17:1, are available for applications with gross axle weight ratings up to 60,000 pounds.
For more information on all Spicer axles and other Roadranger products and services, visit the Internet at http://www.roadranger.com, or write to Roadranger Marketing, P.O. Box 4013, Kalamazoo, MI 49003. To reach a Roadranger right now, dial 1-800-826-HELP (4357) in the U.S. and Canada. In Mexico, dial 01-800-826-4357.
The Roadranger® solution is an unbeatable combination of the best drivetrain, chassis, and safety components from Dana Corporation and Eaton Corporation, all backed by the Roadrangers – the most experienced, most expert, and most accessible drivetrain consultants in the business.
Dana’s Commercial Vehicle Systems group designs, manufactures, and markets front-steer, rear-drive, trailer, and auxiliary axles; driveshafts; steering shafts; suspensions; and related systems, modules, and services for the commercial vehicle market. Major components and modules are marketed under the Spicer® brand name.
About Dana Corporation
Dana is a world leader in the supply of axles; driveshafts; and structural, sealing, and thermal management products; as well as genuine service parts. The company's customer base includes virtually every major vehicle and engine manufacturer in the global automotive, commercial vehicle, and off-highway markets, which collectively produce more than 65 million vehicles annually. Based in Toledo, Ohio, the company's continuing operations employ approximately 35,000 people and reported 2006 sales of $8.5 billion, with more than half of this revenue derived from outside the United States. For more information, please visit: http://www.dana.com/.
Dana and certain of its U.S. subsidiaries are operating under Chapter 11 of the U.S. Bankruptcy Code as debtors in possession. Information about the bankruptcy proceedings can be found at: http://www.dana.com/reorganization. While Dana continues its reorganization under Chapter 11, investments in its securities are highly speculative. Although shares of Dana common stock continue to trade on the OTC Bulletin Board (OTCBB) under the symbol "DCNAQ," the trading prices of the shares may have little or no relationship to the actual recovery, if any, by the holders under any eventual court-approved reorganization plan. The opportunity for any recovery by holders of Dana common stock under such reorganization plan is uncertain and shares of Dana common stock may be cancelled without any compensation pursuant to such plan.
BusCon 2008
Chicago, Illinois
Sep 16, 2008 to Sep 17, 2008
|
|
|
|
|
|