|
* These (950 lbs.ft. - 1750 lbs.ft) transmissions can be rated at 100 additional lbs.ft. torque above the stated limit in the top two ratios only. ** This (950 lbs.ft. - 1750 lbs.ft) transmission can be rated at 200 additional lb-ft. torque above the stated limited in the top two gears only.
|