ServiceRanger

New! We are pleased to announce that ServiceRanger Version 3.0 is now in production. This latest version will support all new and existing Roadranger automated products. This is not an upgrade for previous versions. This is a new application that can be installed without removing ServiceRanger versions 2.x.

 

New Features and Support

  • Local embedded Roadranger Product Configurations\Programming Database stores all programming files. It is no longer necessary to download files from the Eaton web server.  No Username required.
  • Vehicle Components function that shows information about all vehicle components being detected by ServiceRanger.
  • J-1587 and J-1939 Fault Code Detection
  • J-1587 and J-1939 Product Configuration\Programming Support.
  • Data Monitor function now supports both J1587 and J1939 data parameters.
  • Automatic ServiceRanger Update Notification Service.

Current Products Supported (first release)

  •  Vorad VS-400 Collision Warning System
  • Generation 3 Autoshift and Ultrashift Transmissions
  • Hybrid Drivetrain Systems

**Note: Do not un-install ServiceRanger version 2.x at this time. This is not an upgrade for the previous versions of ServiceRanger.  ServiceRanger 2.x is currently still required to support the EVT-300 collision warning systems. ServiceRanger 2.x also still supports current automated transmissions products.**

 

 

Installation\Updates

 

Click on the following link to download. Follow the dialogue pops up, click "Run" or click "Save" to install it at a later time. The file on this page requires the user to have full Administrator Privileges on the computer before the file can be downloaded and installed.

 

Click Here To Install ServiceRanger Version 3.0.5.0

 

 

Software Registration and Unlock Code

 

After the software is installed it will be necessary to register the software and obtain an unlock code to activate the software. Click on the following link to complete registration. Users will get an e-mail notification with unlock code within 48 hours after submitting their registration. For questions about registering users can contact the Roadranger Automated Products Call Center at 1-800-826-4357. Users outside the US and Canada should contact their local Roadranger.  

 

Click Here For Software Registration and Unlock Code 

 

 

System Requirements

 

Operating Systems - Windows 2000      Windows XP    Windows Vista   
CD-ROM Drive

500 MB of free hard drive space

 

 

ServiceRanger 3 User Guide

 

Click on the following link to access the ServiceRanger 3 User Guide.   

 

 

RP-1210 Communications Adapter Support

 

ServiceRanger version 3 supports “Dual Link” connections, meaning it can be configured to support both J1587 and J1939 communications devices. Not all communications adapters support dual link connections. Click on the link below to view a list of communications adapters that have been tested and are “recommended” to be used with ServiceRanger version 3.0.

 

Click Here For RP-1210 Communications Adapter Information