SpeedSense Series Inductive Proximity Sensors
The newly released SpeedSense sensor from Eaton's electrical business is one of the first tubular inductive sensors to feature built-in speed detection technology. This functionality allows the sensor to detect when the target RPM falls under a specified limit.
SpeedSense is not just limited to rotating applications. By measuring the time between two detections, the sensor can fit in a wide variety of applications. When the time between two target detections exceed the rated millisecond limit, the sensor will activate.
SpeedSense is not just limited to rotating applications. By measuring the time between two detections, the sensor can fit in a wide variety of applications. When the time between two target detections exceed the rated millisecond limit, the sensor will activate.
- Built-in speed detection technology activates the sensor when the target’s rotational or lateral speed slows (output “closes” when motion stops)
- Outputs are N.O. by default, but N.C. models can be special ordered from the factory
- Reliably detects metal targets at up to three times range of conventional inductive proximity sensors
- No special programming necessary
- Auto-configure output allows for automatic NPN or PNP
- Resistant to extreme temperature (-40°C) & high pressure washdown
- High electrical noise immunity of 10 V/m
Loading Content..Please wait!
- UL Listed