PV fireman's switch SOL30-SAFETY
The Eaton PV fireman’s switch SOL30-SAFETY disconnects DC cables from the voltage source and facilitates fire-fighting without this electrical hazard.
In the solar PV industry there are major concerns regarding the safety aspects of fighting fires in buildings where there are solar PV systems installed. During the day while the solar panels are actively producing DC power it becomes necessary to quickly and safely isolate the PV panels from the rest of the system in the event of a fire.
The Eaton SOL30-SAFETY fireman’s switch offers maximum safety to firefighters where solar PV systems are installed. The SOL30-SAFETY works by disconnecting the PV panels from the rest of the system as soon as the main AC breaker is tripped or switched by the firefighters. This is achieved by the inherent under voltage release which automatically disengages the SOL30-SAFETY when the AC voltage is not present. The fireman’s safety switch is rated at 1000V DC, 30A and can be manually switched as well.
The Eaton SOL30-SAFETY fireman’s switch offers maximum safety to firefighters where solar PV systems are installed. The SOL30-SAFETY works by disconnecting the PV panels from the rest of the system as soon as the main AC breaker is tripped or switched by the firefighters. This is achieved by the inherent under voltage release which automatically disengages the SOL30-SAFETY when the AC voltage is not present. The fireman’s safety switch is rated at 1000V DC, 30A and can be manually switched as well.
Loading Content..Please wait!