MARINA GROUND FAULT MONITOR
ground fault monitorOur ground fault monitoring systems are designed to detect fault currents in the AC shore power system that are too low to trip a circuit breaker. It helps reduce the risk of injury or property damage which may result from stray fault currents. It provides information to the maintenance staff on the overall condition of the AC electrical system.
 
Buy Now!

  • UL Listed Current Transformers
  • Adjustable Trip Level 10mAmps to 10 Amps
  • Current Transformers up to 8 1/4” Diameter
  • Visual and/or Audible Alarm
  • Housing of Fiberglass, or Powder Coated Stainless Steel Available
Loading Please wait..
  • Power Guard
    The ground fault monitor detects ground fault currents by means of current transformers (CT), which are placed around main or branch circuits. If a ground fault occurs, the CT will detect the amount of fault current and send a signal to the ground fault monitoring device where the amount of fault current is displayed with the faulty circuit identified. The detected fault can either activate an indicator alarm or disconnect the faulted circuit.
149 Warwick Court
Williamsburg, VA 23185
Toll Free: (800) 723-8009
Phone: (757) 258-8800
Fax: (757) 258-8805
emailmarinasales@eaton.com
rvsales@eaton.com