Download & Updates
The files on this page require the user to have full administrator privileges on the PC before these files can be downloaded and installed. Note that some companies do not allow their users to download files from the Internet. If you are not sure, or have issues downloading or installing any of the files on this page, contact your local computer or network administrator for more information.
- ServiceRanger 2.80 (August 2011)
- ServiceRanger 3.0
- Hydraulic Launch Assist (HLA) Advanced Product Function - please call the Roadranger help desk at 1-800-826-4357
- Service Bulletins & Update Information
- ServiceRanger Version 2 Users Guide
- ServiceRanger Version 3 Users Guide
- Eaton MD-100 Communication Driver (version 1.06)
Contains the latest RP-1210 communication drivers for the Eaton MD-100 Vehicle Link Adapters (MD-111-CT and MD-111-W). - Microsoft .NET version 2.0 Install
Required for ServiceRanger version 3. Install if when installing SR3 you are prompted that Microsoft .NET is not installed on your computer. - Microsoft DAO 3.5 Install
Installs the Microsoft Data Access components required for ServiceRanger version 2 and Eaton MD-300 Heavy Duty Diagnostics software. Install this patch if you get a database error message at startup.