Feb 2011
Are Your Aftermarket Parts EverTough?
Eaton has launched a new brand of replacement components engineered specifically for the aftermarket. The new lineup, known as EverTough™, provides aftermarket customers with the optimum balance of price and performance to meet their replacement part needs. The initial EverTough component offering is a new line of heavy-duty clutches. To ensure the new EverTough clutches have reliability and durability at a competitive aftermarket price, Eaton has designed the clutch with an aftermarket-specific facing, a release system with standard dual zerk fittings, and dampeners to meet the torsional vibration needs of the aftermarket. For more information visit EverTough.com
Dana Introduces Service Free U-Joint for Spicer Life Series® Driveshafts
Dana has announced the introduction of service-free u-joints to its heavy-duty Spicer Life Series® (SPL®) driveshafts. This technology delivers a permanently lubricated driveline that reduces maintenance costs over the life of the product. The new design is available for SPL-250 and SPL-170 series and have been designed for main and tandem drive inter-axle driveshaft applications. The Spicer Life Series features a new bearing package that includes larger needle bearings for increased capacity, a special Viton® synthetic seal for improved grease retention, and a thermoplastic seal guard to exclude contaminant. These features will come standard on SPL service free u-joints and will be available to all OEM's in March of 2011.UltraShift PLUS Provide Smoother Shifting for Wyoming DOT
Maintaining roughly 16,000 lane miles of road surface in a state that can see as much as 200 inches of snow annually is no small task. But that’s exactly what the Wyoming Department of Transportation (WYDOT) does with a fleet of 3,000+ trucks. When the WYDOT fleet director needed to replace nearly three dozen snow plows within his fleet, he decided to upgrade from Eaton’s AutoShift automated transmission series to its latest generation of UltraShift PLUS automated transmissions.The result: improved efficiency and reliability, driver recruitment and performance.
Get the full story on UltraShift PLUS in the WYDOT fleet.
Guaranteed payment without calling Real Time!
Roadranger has over 20 pre-authorized repairs that can save you time on the phone. For guaranteed payment:- Follow the guideline repair and labor parameters.
- Reference the pre-authorized guideline number in the claim text. This number can be used in place of a RTW number.
Pre-Authorized - External Heat Exchanger (Cooler) Failure - Repair Guideline
Pre-Authorized - Internal Heat Exchanger (Cooler) Failure - Repair Guideline
Pre-Authorized - Lightning Splitter Cylinder Oil Ingestion - Repair Guideline
Pre-Authorized - Splitter Complaints - Fault Code 42 - Repair Guideline
Pre-Authorized - Broken Damper Spring - 7 Spring Damper - Repair Guideline
For ease of use, pre-authorized guidelines are all contained in a single document that can be downloaded for review (TCWY1250). This document can be downloaded using the link below.
Click here to access a complete list of Pre-Authorized Repairs.
Did you know?
Calling Real Time Warranty is only REQUIRED for Eaton Hybrid Products. Calling Real Time Warranty is NEVER required for Automated Transmissions, Manual Transmissions, Clutches, and Axle Products!
Core Change Update
As of January 19, 2011 Eaton has reinstated the core value assigned to the Gen 2 REMAN Exchange Transmission Controller Kits. Core reimbursement for aftermarket and warranty returns will continue to follow the OEM core reimbursement guidelines.
| New Core Charge added to the Controllers listed below |
||
| Eaton Part No. |
Part Description |
Core Value |
| K-3435RX |
REMAN Exchange Transmission Controller Kit |
250.00 |
| K-3439RX |
REMAN Exchange Transmission Controller Kit |
250.00 |
| K-3443RX |
REMAN Exchange Transmission Controller Kit |
250.00 |
| K-3444RX |
REMAN Exchange Transmission Controller Kit |
250.00 |
| K-3445RX |
REMAN Exchange Transmission Controller Kit |
250.00 |
| K-3449RX |
REMAN Exchange Transmission Controller Kit |
250.00 |
| K-3457RX |
REMAN Exchange Transmission Controller Kit |
250.00 |
| K-3505RX |
REMAN Exchange Transmission Controller Kit |
250.00 |
| K-3516RX |
REMAN Exchange Transmission Controller Kit |
250.00 |
| K-3639RX |
REMAN Exchange Transmission Controller Kit |
250.00 |
| K-3557RX |
REMAN Exchange Transmission Controller Kit |
250.00 |