Select your location

New Eaton Cummins Powertrain Geared for Mexico

Date: November 15, 2017

GALESBURG, MI … Eaton Cummins Automated Transmission Technologies has introduced a new fuel economy-focused calibration specifically designed to meet and exceed the distinctive demands of the Mexican commercial trucking industry. The newly configured 18-speed Eaton UltraShift PLUS ® MXP automated transmission will be paired with a Cummins ISX15 diesel engine, delivering a powertrain designed for premium performance and maximum fuel efficiency in Mexico’s unique driving conditions.

“We collaborated with local Eaton, Cummins, and customer experts to analyze duty cycles and fuel economy requirements for the region,” said Alex Stucky, product strategy manager, linehaul, Eaton Cummins Automated Transmission Technologies. “We then took the UltraShift PLUS MXP transmission, which is typically targeted for highly demanding and rigorous applications, and developed fuel economy calibrations optimized to the Cummins ISX15 engine models available in Mexico.”

Stucky added that more than 100 key parameters were analyzed, modified and tuned on the UltraShift PLUS MXP automated transmission. These included alterations to downshift points, upshift points, retarder limits, demand modulations, acceleration pedal tuning, and grade offsets while leveraging MXP gear ratio coverage to maintain engine efficiency. The new powertrain package will be available as a service release in December, with production availability in the first quarter of 2018.

The joint venture’s newest integrated powertrain offering is available with IntelliConnect™ for fleets in Mexico using Geotab web-based analytics. IntelliConnect is a telematics capable system that provides near real-time monitoring of vehicle fault codes, prioritizes the critical events and provides accurate and comprehensive action plans by technical experts at Eaton.

The joint venture’s components are backed by Eaton’s Roadranger network of more than 180 drivetrain professionals who provide solutions, support and expertise to fleets and dealers. For more information visit www.eaton.com/roadranger, where the latest product information is available, as well as service, parts and training assistance, 24 hours a day. Experts are available in the Roadranger Call Center by dialing 1-800-826-HELP (4357) in the U.S. and Canada. In Mexico, dial 01-800-826-4357.

Eaton Cummins Automated Transmission Technologies is a 50/50 joint venture between Eaton (NYSE: ETN) and Cummins, Inc. (NYSE: CMI)). The global joint venture produces industry-leading medium- and heavy-duty automated transmission technologies, and markets, sells, and supports Eaton’s current and next generations of automated medium- and heavy-duty transmissions to OEM customers in North America.


Contact US
Jim Michels
(248) 226-6806