Download document () of 20
We make what matters work

How to meet regulations for emergency lighting

Standard regulations for emergency lighting

To ensure that emergency lighting is fit for purpose a combination of standards and regulations covers all aspects of its safety.  Using a third party to certify a system is an effective way of helping to ensure quality, reliability and conformity.

A key element of the compliance landscape is the EN50172 standard. This sets out the requirements for emergency lighting when the supply to all or part of the normal lighting in occupied premises fails. It states that emergency lighting shall: 

  • Indicate escape routes clearly and unambiguously 
  • Provide illumination along such routes to allow safe movement towards and through the exits provided
  • Ensure that fire alarm call points and firefighting equipment provided along escape routes can be readily located
  • Permit operations concerned with safety measures.

Example European standards framework

Legislation
(legal requirement)
National fire safety legislation
Harmonised EU
Application standards (shall)
EN 50172
Emergency escape systems
EN 1838
Lighting applications, emergency lighting
Harmonised EU
Protected standards (shall)
EN 60598-2-22
Luminaires for emergency lighting
EN 60235
Automatic test systems
EN 50172
Central power supply systems

Exit sign format

Time is of the essence during evacuation and this means it is critical that all escape route signage can be quickly seen, understood and followed. Section 4.1 of EN1838:2013 details this point stating that ‘Signs which are provided at all exits intended to be used in an emergency and along escape routes shall be illuminated to indicate unambiguously the route of escape to a point of safety’. 

Where there is no direct sight of an emergency exit, an illuminated directional sign or series of signs must be provided to help people make their way to the emergency exit. The single pictogram format specified in ISO 7010 and adopted by many national standards bodies from 2011 onwards is current best practice.

Most countries have adopted pictogram style signs, or are in the process of updating local guidelines.

usa-emergency-exit-sign-focus.png
The most notable exception is the USA where green or red glowing "EXIT" letters are commonplace.
  Progress left Progress forward Progress right
Recommended signage 
EN ISO 7010:2012 E002
Accepted signage

Legacy signs 

 

Exit sign colour and illumination

ESCAPE route sign colours are specified by ISO 3864 that:

  • Exit and first aid signs must be white, with green as the contrast colour
  • White to green luminance ratio must be between 5:1 and 15:1.
  • Minimum luminance of any 10mm patch area on the sign must be greater than 2cd/m
  • Ratio of maximum to minimum luminance must be less than 10:1 for either colour. 
emergency-lighting-self-contained-example-of-poor-visbility.png
Badly illuminated exit sign
emergency-lighting-self-contained-example-of-good-visbility.png
Well illuminated exit sign

Locating safety luminaires at points of emphasis for emergency evacuation

Every system design must correctly locate luminaires to reveal specific hazards and highlight safety equipment and signs – known as points of emphasis – whether it is for an emergency escape route or open (anti-panic) area. The design must also take into account the type of luminaire needed and its light output as detailed by EN 1838: 2013 and EN 60598-2-22. The following representation highlights key points of emphasis requiring a luminaire:

Seven points of emphasis to consider when locating safety lights

The following representation highlights key points of emphasis requiring a luminaire:

points-of-emphasis-for-safety-lights.png

Maximum viewing distances for escape signs

internally-illuminated-exit-sign-200-panel-height.png
Internally illuminated signs – 200 x the panel height
externally-illuminated-exit-sign-100-panel-height.png
Externally illuminated signs – 100 x the panel height

Maximum viewing distances and luminance conditions are detailed for all safety sign formats in EN 1838: 2013. Signs can either be internally illuminated – such as exit boxes or edge-lit emergency luminaires with a screened sign that have a controlled illuminance – or be of a non-powered type. 

While internally illuminated exit signs that meet EN 60598-2-22 are pre-tested to ensure compliance, extra care must be taken if the sign is designed to be externally illuminated. An emergency luminaire must be sited within 2 metres of the sign and the multiplication factor is only 100. The sign must be illuminated to a minimum lux on any part of its face in emergency conditions.

How to plan emergency ESCAPE routes

Once the points of emphasis have been covered, designers must consider if any additional luminaires are needed to ensure minimum illuminance levels so that routes can be used safely. Every escape route compartment must have at least two luminaires in case one should fail. 

Lighting level requirements

A minimum lux is required on the escape route centre line as detailed by EN 1838: 2013 4.2. A uniformity ratio of 40:1 maximum to a minimum must not be exceeded. 

This illuminance must be provided for the full duration and life of the system. A % of the illuminance must be available within five seconds and full illumination must then be supplied within a specified time period following supply failure. 

escape-route-lighting-requirements.png

Photometric design

Authenticated spacing tables or a suitable computer program are used to determine whether luminaires are needed beyond those at points of emphasis to provide the minimum required level of illumination on escape routes. 

To ensure that the design will meet the required levels at all times the data is ‘de-rated’ – as required by the standard – to take into account:

  • light reduction as battery voltage reduces during discharge 
  • ageing of lamps in maintained circuits
  • the effects of dirt
minimum-illumination-not-met-for-emergency-lights.png
Luminaires at points of emphasis (minimum illumination not met)
building-plan-with-1-lux-minimum-safety-lighting.png
Additional luminaire to achieve 1 lux minimum

Open (anti-panic) core areas

An ‘open (anti-panic) area’ is so defined if it is larger than 60m2, has an escape route passing through it or it features hazards identified by the building risk assessment. The current standard makes it straightforward to design and verify systems that provide good uniformity, rather than using a small number of large-output luminaires. 

Light level requirements

A 0.5 lux minimum of the empty core area – which excludes a 0.5m border of its perimeter – is detailed by EN 1838:2013 – 4.3. Spacing table (example below) or a suitable computer program are similarly used to generate data. This is then de-rated in the same way as it is for escape route lighting to determine luminaire location. 

Spacing data 

Spacing tables provide photometric data which can be used to help ensure that the emergency lighting system has been designed correctly and meets the required illumination levels.

open-area-anti-panic-safety-lighting-example.png

High-risk locations

The risk assessment will identify any locations needing special consideration. For example, these might include plant and production lines deemed to be high risk or control rooms that manage dangerous processes. 

For these high-risk areas, EN 1838: 2013 details that the maintained illuminance on the reference plane shall not be less than 10% of the required maintained illuminance for that task and never less than 15 lux. 

Design implications

When designing for areas that require enhanced levels of emergency illumination, it’s important to consider all the options which may include converted mains lighting, self-contained or CBS-powered luminaires. In most cases, the solution will also have higher Ballast Lumen Factors (BLF). 

Emergency response time is another critical factor for high-risk locations. This may require emergency luminaires to be operated in maintained mode or alternatively the use of tungsten projector units. Should the latter be chosen, it’s important to bear in mind the need to maintain a reasonable level of uniformity.

emergency-lighting-in-high-risk-locations.png

This way to safety

Get the full picture - download your free emergency lighting fundamentals guide

In our comprehensive guide, we delve deeper into Emergency Lighting design considerations. From conforming to regulations to considering illumination distances and how to combine items to make a complete system.

Start with the emergency lighting leader

Emergency lighting market leader Eaton offers more than 50 years of expertise built up through a brand heritage that embraces CEAG, Luminox, Blessing Menvier, JSB, Crompton and Univel. We work closely with national and international industry organisations to achieve the highest standards of regulatory compliance, safety, reliability and efficiency.