Eaton powers up telescopes at Siding Spring Observatory

 

Date: 2019/10/21

Segment: Buildings and Commercial

Location: NSW, Australia

 

Located on the edge of the picturesque Warrumbungle National Park in New South Wales, Siding Spring Observatory is Australia's premier optical and infrared astronomical observatory with 5 unique telescopes. They are part of a global network of observatories which allows researchers to track a star in the sky 24 hours per day, 7 days per week.  

Image of SSO.jpg

University collaborations allow the observatory to globally facilitate a variety of research, from probing the depths of the cosmos in search of "Dark Energy" to searching the Milky Way for other planets and signs of life.

Each telescope is unique, varying in size and capability, with some able to see fainter objects and others able to move faster through the sky, facilitating different observations and new discoveries.   

When the back-up power system for one of its largest telescopes was coming to the end of its life, Siding Spring Observatory decided to upgrade its technology.

Protection for all conditions

Mark Willis, Siding Spring Observatory Site Manager is responsible for maintenance, upgrades and breakdowns at Siding Spring Observatory.

He is tasked with implementing a global maintenance plan which tests equipment and implements necessary upgrades every 18 months. A preventative maintenance plan also ensures the emergency backup system is tested every 12 months. This is to give the team confidence that in the event of power loss, the backup generator will work as intended.

One of the telescopes, a 2-metre equatorially mounted telescope, is much larger than the others. It has a hydraulically operated roof that can open and close multiple times per night. If the roof is open and there is loss of AC mains, there is an emergency backup DC Power System complete with batteries that close the roof.

One night, researchers at Siding Spring Observatory opened the roof of the telescope to view the night’s stars. When they were finished, they noticed that the roof of the telescope would not close.

“This really alarmed the researchers at the observatory as any rainfall could cause huge damage to this multi-million-dollar equipment. After some testing, we found that it was the batteries in the backup Power System that failed to close the roof of the telescope,” said Mark Willis.

Choosing a reliable partner

Mark was aware that their old 48v DC power backup system was 15 years old and the batteries were nearly due to be replaced. He decided that it was a good opportunity to install a more modern system. Mark approached Natural Power Solutions as they are a trusted provider of other Uninterruptable Power Supplies (UPS) to the site. Natural Power Solutions recommended that Eaton’s DC power backup system was the best fit for the observatory.  

“All of the observatory sites run Eaton AC UPS’s globally, so we trust their power systems. Another thing we really value is their backup support. This is what ultimately led us to choose them as our supplier of power backup system,” said Mark Willis, Siding Spring Observatory Site Manager.

Eaton’s DC Power backup System (48V) was chosen to backup the emergency hydraulics motor for the telescope.

A local build

“This telescope is unique in that it is the only one on this site that needs backup power to the large AC motor that opens and closes it,” said Patrick Staunton, Sales Engineer at Eaton. “This is to ensure that in the event of a power outage, the backup DC motor will kick in and ensure the roof can still close.”

The DC power backup system that Eaton manufactured works in tandem with a PLC/hydraulic control panel in order to know when to close the roof.

“The solution required a lot of intelligence and so we carried out configurations on site ensure that the software was configured to know when the roof should open and close, what time it should operate at and when it is fit to operate,” said Patrick Staunton.

Eaton custom built the DC power backup system in a couple of weeks and installed it over the course of four days.  The system had multiple components including batteries, system SC200 controller, rectifiers, and Eaton configured additional features via software which provided safe operation and monitoring.  

“Having to get all inputs and outputs done and systems integrated takes a lot of time but thankfully, Eaton manufactured the DC Power System locally and so it only took a couple of weeks to build. This was a key advantage for Eaton as it resulted in a much shorter lead time,” said Mark Willis.