Even a momentary blip in availability "would not only adversely affect out business, but it would affect our customers' confidence in us."
With Eaton's Power Xpert 9395 in place, Atlantic.Net is able to...
Atlantic.Net discovered everything it was seeking in the 9395 UPS. The company chose an 825 kVA model, comprised of three modules providing N+1 redundancy, gaining the ideal level of protection it was seeking.
The 9395's unprecedented combination of power performance, reliability and efficiency provides the highest availablility on the market -- in part due to its inherent redundancy option, which allows the unit to be configured so its uninterruptible power modules automatically act as N+1 redunanct systems.
“We have made a substantial capital investment in our power infrastructure and it is very important to us that we are able to get a return on investment on this. It is too early to know firm facts and figures on what our savings will be, but we are looking at saving at least 10 percent over our prior installation due to the efficiencies that have been introduced by the 9395.”
Atlantic.Net also utilizes Eaton’s Power Xpert enterprise software, which offers system level management of power infrastructure via a web browser, from any desktop, on one screen. The software provides access to critical information from any location. “I’m amazed by the different levels of detail and the reports we are able to obtain,” Haines adds.
Power Xpert allows users to customize the conditions under which alarms are triggered — including firstline and escalations — making it easy to identify which device is in alarm and where it is located.
To ensure optimal performance of its UPS solution, Atlantic.Net relies on an Eaton service plan, which includes regularly scheduled preventive maintenance calls .“We need to guarantee 100 percent uptime for our customers, so a service plan is crucial for us to ensure that our units are 100 percent healthy,” Haines explains.
The 9395’s small footprint— up to 60 percent less than competitive units —was ideal for Atlentic.Net, with the unit occupying minimal real estate in its data center. “The footprint has been drastically reduced compared to the replacing unit,” Haines confirms
As Atlantic.Net’s power needs increase, the 9395 can be expanded in building-block increments by adding additional modules, eliminating the need to purchase a new UPS. This advantage not only contributes to the solution’s maintainability, but is especially valuable to the firm whose customer base is constantly expanding.