Eaton launches new series of deck hangers to help reduce installation time and simplify electric code compliance

Date: February 7, 2017

HIGHLAND, IL — Power management company Eaton today announced a new series of deck hanger brackets designed to reduce labor while meeting critical electrical code requirements through a robust riveted assembly and identical ends that do not require the installer to identify proper side prior to installation. 

The new B-Line series deck hanger brackets provide the minimum conduit standoff to meet the National Electrical Code (NEC) section 300.4(E) that states that cables and raceways must be installed at least 11/2” (38 mm) under decking to prevent potential damage from nails or screws. 

“With a unique same end design, Eaton’s B-Line series deck hanger bracket simplifies the install, allowing for a quicker install, while meeting the NEC code minimum for conduit standoff on deck hangers,” said Amelia Grattan, product line manager, Eaton’s B-Line Division. 

Eaton’s B-Line series deck hanger bracket supports conduit or pipe up to 1-1/2” diameter, and is Underwriters Laboratories® (UL) listed in the United States and Canada as a hanger up to a 250 lb. static load. Eaton’s S18 assembly also includes Guide Rite™ conduit and electrical box support hanger, which helps ensure proper support of boxes and conduit per NEC requirements.

For more information, visit www.eaton.com/deckhanger.

Eaton’s electrical business is a global leader with expertise in power distribution and circuit protection; backup power protection; control and automation; lighting and security; structural solutions and wiring devices; solutions for harsh and hazardous environments; and engineering services. Eaton is positioned through its global solutions to answer today’s most critical electrical power management challenges.

Eaton is a power management company with 2017 sales of $20.4 billion. We provide energy-efficient solutions that help our customers effectively manage electrical, hydraulic and mechanical power more efficiently, safely and sustainably. Eaton is dedicated to improving the quality of life and the environment through the use of power management technologies and services. Eaton has approximately 96,000 employees and sells products to customers in more than 175 countries. For more information, visit Eaton.com.

Contact 
Ann Marie Halal, (440) 523-4418
Regina Parundik, (412) 559-1614