The solution has been developed in close collaboration with
Fortum, a leading energy provider in the Nordic and Baltic countries. Extensive testing between Eaton and Fortum has proven that the UPS can work as part of a virtual power plant to enable data centers to take part in the high-value
Frequency Containment Reserve (FCR) and demand-side market. The UPS can be used to regulate demand from the grid, as well as for up and down stream charging, to discharge the battery back to the grid. Eaton’s UPSaaR solution gives data center operators, such as colocation and cloud service providers, an opportunity to work with energy providers to momentarily reduce the power demands of the data center, return power to the grid and be compensated for adjustment to power consumption. This helps the grid avoid power outages, without compromising critical loads.