A medium-voltage distribution transformer or service transformer is a transformer type that provides the final voltage transformation in the electric power distribution system, stepping down the voltage used in the distribution lines to the level used by the customer.
Practical levels of voltage are often referred to as medium voltage, meaning the incoming voltage to the transformer is in the order of 5 kV to 35 kV. Some distribution voltages may exceed 35 kV and would be considered high voltage, but most of the distribution system is within the medium-voltage range. Modern distribution transformers are manufactured in accordance with many standards, most notably by IEEE (Institute of Electrical and Electronics Engineers) and IEC (International Electrotechnical Commission).
In the United States, the features and functionality of most distribution transformers fall under IEEE standard C57.12.00 (Standard General Requirements for Liquid-Immersed Distribution Power and Regulating Transformers), however, there are a multitude of standards that apply to specific types and applications of transformers, including substation type, compartmental pad-mount type, single-phase, pole-mounted transformers, generator-duty transformers, high-temperature transformers and many more.
The substation transformer is the heart of the electrical substation. This transformer changes the relationship between the incoming voltage and current and the outgoing voltage and current. Substation transformers are rated by their primary and secondary voltage relationship and their power-carrying capability. For example, a typical substation transformer would be rated 15 kV, 25 kV, 35 kV or 46 kV on the primary at a power rating of about 5–20 MVA. The secondary or low voltage can be 15 kV down to 5 kV or even less than 600 V. Substation-style transformer design and functionality is dictated by IEEE standards C57.12.00 and C57.12.36. These types of transformers consist of a core and coils immersed in oil or dielectric fluid in a steel tank. The oil or fluid serves both as an insulator and as a coolant to keep the core at reliable operating temperatures. Substation units are easily identified by their exposed bushings, gauges, panels or monitoring equipment and are typically located behind a fence or within a restricted area.
A three-phase pad-mounted transformer is a ground-mounted electric power distribution transformer in a locked steel cabinet mounted on a concrete pad. These types of transformers are generally smaller (45–5000 kVA) but can be produced at larger station sizes as well (up to 10 MVA). These are installed in locations near or within public areas. The compartmental, tamper-resistant, pad-mounted transformer design makes it ideal for applications where public safety is imperative. The overall design and functionality is dictated by IEEE standard C57.12.34, while the tamper-resistant nature of the pad-mount transformer is dictated by IEEE standard C57.12.28 or C57.12.29 for coastal areas.
Single-phase pad-mounted transformers are commonly installed in residential areas and are intended for power distribution through underground systems. Features and layout of single-phase pad-mounted transformers can be found in IEEE standard C57.12.38. These transformers are typically rated 10–167 kVA (up to 250 kVA as per scope of IEEE standards) and up to 35 kV on the primary.
Single-phase pole-mounted transformers are frequently installed in residential areas but can also be common for small businesses requiring three-phase power from a bank. These transformers can vary in size, from as small as 5 kVA to as large as 500 kVA, with voltages up to 35 kV line-to-line. Pole-mounted transformer banks allow three single-phase units to be connected to a three-phase system to distribute through overhead lines. Winding connection styles, mounting standards and overall layout and functionality are held to IEEE standard C57.12.20.
Ventilated dry-type transformers are voltage changing (step-up or step-down) or isolation devices that are air-cooled rather than liquid-cooled. The transformer case is ventilated to allow air to flow and cool the coil(s). For outdoor operations, a dry-type transformer enclosure will usually have louvres for ventilation. Dry-type transformers adhere to IEEE standards C57.12.01 and C57.12.91, with ratings from 15 kVA to 30 MVA, and primary voltages above 601 V.
Ratings are the fundamental blueprint for describing the performance characteristics and style of a transformer.
Standard ratings for types of distribution transformers are found in IEEE product standards, including the following:
kVA: transformers are rated in kilo-volt-amperes (kVA). kVA is used to express a transformer rating because not all transformer loads are purely resistive. The resistive component consumes power that is measured in watts, whereas the reactive component consumes power measured in VARs. The vector sum of these two loads is the total load, VA or kVA
Voltage: the voltage designation defines both the way a transformer may be applied to a system and the transformer design. IEEE Std C57.12.00 defines the designation of voltage ratings of single and three-phase transformers.
Voltage designation examples:
Three-phase
Single-phase
Temperature rise: a kVA rating is based on the current that the transformer can carry without exceeding its temperature-rise rating. The more heavily loaded a transformer becomes, the higher its internal temperature gets. The maximum temperature rise that the transformer can withstand without abnormal loss of life is governed by customer specifications or by IEEE standards
Fluid: for over a century, transformers have used conventional mineral oil as a dielectric coolant. It offers reasonable cost with proven, reliable, long-term performance. Maintenance procedures are well established and used mineral oil can usually be reconditioned for use by filtering and degassing. The fire point of mineral oil is approx. 155°C, while the fire point of a less-flammable fluid is above 300°C. This makes less flammable fluids, such as Envirotemp FR3, the better alternative for installations indoors, on top of buildings or in high pedestrian traffic areas. Use of less-flammable fluids is recognised as a method of reducing fire hazard, indoors and outdoors, by the National Electrical Cod (NFPA 70) and the National Electric Safety Code
| Key ratings |
| kilo-volt-amperes (kVA) |
| Primary voltage |
| Secondary voltage |
| Basic insulation level (BIL) |
| Impedance |
| Frequency |
| Cooling type |
| Temperature rise |
There are two distinct choices for high-voltage connection of a transformers.
Live-front (porcelain type): the voltage-carrying parts are exposed. Livefront terminations have high-voltage connectors, arresters or fuses are exposed to the operator after cabinet has been opened.
Dead-front (separable insulated connector type): often referred to as deadfront bushings. Safety is enhanced as there are no current-carrying parts exposed to the operator.
Deadfront connectors fall into two main categories: loadbreak and deadbreak.
There are two basic types of distribution system configurations:
These system configurations can be used alone or in combination with one another on different portions of the distribution system. Complex combinations are sometimes referred to as networks consisting of radial and loop branches with multiple sources of supply.
Radial system
A radial system employs one dedicated transformer to serve a customer or group of customers. The drawback is the fact that if there is a failure in the distribution line, all of the customers downstream from the problem are without power. In the below example, the transformers are shown with fuses, which would isolate them from the distribution line in the event of an overload or transformer failure. Radial systems are mostly used in rural or remote areas. Radial feed systems require transformers to have only one high-voltage bushing per phase line to be connected (one for grounded wye applications and two for delta and wye applications), since no current is being looped through any transformer.
Loop system
A loop system is fed by two different feeders – one connected to each end of the loop. Theoretically, the entire loop of transformers could be fed by either source, or the transformers can be split up between the two sources, depending on where an “open point” is created. In the event of a failed underground cable, this open point is “moved” (by using load-break switches or elbows), so that no customers are out of power while the cable is repaired. In the below example, the transformers are shown with fuses, which would isolate a failed transformer, limiting the outages to those customers fed by the failed transformer. Loop feed transformers have two high-voltage bushings per phase line being connected, so current can loop through the transformer, downstream to the next one.
The purpose of this standard is to describe the requirements for enclosure integrity of pad-mounted equipment that provides long field life with minimum maintenance and resists tampering.
Enclosure security
The plan view shows the ANSI segments used to identify the location of both the high-voltage and low-voltage bushings.
Segment 1 (front): nameplate, gauges, valves, etc.
Segment 2: standard for wall-mounted bushings (optional segment 4)
Segment 3: standard for cover-mounted bushing
Segment 4: standard for wall-mounted bushings (optional segment 2)
Cooling types
There are many types of transformer protection available. They are specified to protect the transformer itself, other equipment and even the safety of nearby people and property. Many of these protections might be required by code.
Main types of protection
There are many variations of these items that are tailored to different types of transformer arrangements. These transformer protective devices, when coordinated with upstream and downstream protection, can protect from a full range of events and help to minimise outages caused by those occurrences by localising the disruption or shutting down the system for higher severity.
Overcurrent protection
Overcurrent protection from fault conditions and overloading can be accomplished with various types of fuses and breakers. Sometimes these will be used in combination with each other and they often need to be coordinated together as a system to get a proper protection and functionality.
Overvoltage
Distribution transformer testing is performed in accordance with the routine testing set forth by the IEEE standards committee, specifically outlined in IEEE standard C57.12.00 with procedures and methodology outlined in IEEE standard C57.12.90.
There are two types of test categories:
Ratio, polarity and phase-relation test
Resistance test
Insulation power factor test
Quality control (QC) impulse test
Core loss (no load loss) and percent exciting current test
Induced potential (OX) test
Winding loss (load loss) and percent impedance test
IEEE impulse test (reduced wave, two chopped waves, full wave)
Temperature (heat run) test (refer to IEEE standard C57.12.90)
PEAK transformers provide increased overload capacity or a smaller, lighter footprint
PEAK transformers are uniquely designed to provide additional capability for managing increased loads and temporary overload capacity.