Eaton UPS Companion V2.2 - Release Note January 2025 =============================================================================== New features: ============= * Add compatibility with the new UPS Eaton 3P Ellipse Cybersecurity: ============== * Nothing. Corrected problems: =================== * Fix the shutdown parameter modification without requiring the software application restart. Eaton UPS Companion V2.1 - Release Note June 2023 =============================================================================== New features: ============= * Add compatibility with the new UPS Eaton 5E G2 Cybersecurity: ============== * Nothing. Corrected problems: =================== * System Tray Icon compatible with system dark theme. * Fix minor bugs Eaton UPS Companion V2.0 - Release Note August 2022 =============================================================================== New features: ============= * New UI / UX redesign of the entire Software. * Add compatibility with the new UPS Eaton 3S 550 & 850 Aus models. Corrected problems: =================== * Fix Events Log display issue. * Fix some translation labels. Eaton UPS Companion V1.07 - Release Note September 2020 =============================================================================== New features: ============= * Add compatibility with the new UPS Eaton 3S 600 & 850 CN models Eaton UPS Companion V1.06 - Release Note March 2020 =============================================================================== Cybersecurity: ============== * Fix for 'Eval Injection' to prevent any vulnerability during software update process Eaton UPS Companion V1.05 - Release Note September 2019 =============================================================================== New features: ============= * EUC compatible with the new version of Eaton 3S Corrected problems: =================== * Display issue on currency value is fixed * User Interface improvements * Default Folder name for EUC installation change to "Eaton" =============================================================================== Eaton UPS Companion V1.04 - Release Note June 2015 =============================================================================== Corrected problems: =================== * Fix issue on upgrade procedure * UAC enable EUC Systray start/stop impossible * Activation Systray with UAC enable =============================================================================== Eaton UPS Companion V1.03 - Release Note Febuary 2014 =============================================================================== New features: ============= * UPS Compatibility: - Eaton 5E Corrected problems: =================== * Nothing Known issues: ============= * Nothing =============================================================================== Eaton UPS Companion V1.02 - Release Note Febuary 2013 =============================================================================== New features: ============= * UPS Compatibility: - Eaton 5S - Eaton Ellipse PRO Corrected problems: =================== * Nothing Known issues: ============= * Nothing =============================================================================== Eaton UPS Companion V1.01 - Release Note December 2012 =============================================================================== New features: ============= * Microsoft Windows 8 and Windows server 2012 compatibility Corrected problems: =================== * Nothing Known issues: ============= * Nothing ================================================================================ Eaton UPS Companion V1.00 - Release Note July 2012 ================================================================================ * UPS Compatibility: - Eaton 3S - Eaton Ellipse ECO - Ellipse - Ellipse MAX - Nova AVR - Protection Station - Protection Center * Supported Languages - English - French - German - Italian - Polish - Portuguese - Russian - Spanish * Known issues - When Windows "User Account Control" (UAC) is enabled, the system tray icon menu fails to send command. Use start and stop commands from Eaton Windows "Start" menu. - When Windows "User Account Control" (UAC) is enabled, the system tray notification setting could also fail to start or stop the notification application. A restart of session after setting should solve the problem. - The manual reset of energy counter should be effective only after a restart of UPS Companion service. - The setting of energy cost will be display in status panel after closing and re-opening UPS Companion display.