Dokument herunterladen () von 20
Wir setzen um, was wirklich zählt.*

NETTERSHEIM, GERMANY … With more choices now available, Eaton’s MAX-LOAD PEXL pleated filter bags give industrial processors a smarter way to cut downtime and improve filtration performance. The enhanced MAX-LOAD PEXL range benefits from a fully welded polyester design that provides broad chemical compatibility and minimal contamination risk. Built for the toughest jobs, the filter bags feature thermo-bonded seams and a smooth outer cage that allow for bypass-free operation and efficient maintenance processes.

At the heart of this innovation is Eaton’s pleated media structure, which offers up to four times more surface area—and up to 10 times more dirt-holding capacity—than standard needle felt bags. This allows for longer runtimes, fewer disruptions and strong performance across a wide range of industrial processes.

“Whether it’s a heavily loaded chemical stream, a hot parts-washing line or a condensate loop, the expanded MAX-LOAD PEXL range gives processors the confidence that their filtration can handle the job,” said Wim Callaert, Senior Product Manager at Eaton’s Filtration Division.

“The use of polyester media provides excellent resistance to acids, alkalis and mineral-oil-based fluids, and that’s why it’s often the go-to for elevated temperature environments where polypropylene would fall short. It’s about giving operators a scalable solution that withstands mechanical and thermal stress without breaking down or bypassing.”

Designed to fit Eaton standard size 01 and 02 housings and backed by the patented SENTINEL® seal ring for true bypass-free performance, MAX-LOAD PEXL filter bags are available in multiple nominal retention ratings from 1 to 50 microns.

With proven durability at temperatures up to 275°F (135°C) and excellent resistance to aggressive fluids and turbulent flow, MAX-LOAD PEXL filter bags are made for demanding filtration setups. In systems where dirt load is high and maintenance windows are limited, they offer a longer-lasting, more capable alternative to conventional needle felt

eaton-max-load-pexl-filter-bag.jpg
Eaton’s MAX-LOAD™ PEXL extended-life thermo-bonded pleated filter bags offer solutions to a wide range of applications requiring dramatically increased capacity applicable in all industrial processes.

About Eaton’s Filtration Division:

Eaton’s Filtration Division is a leader in liquid filtration that can help companies improve product quality, increase manufacturing efficiency, protect employees and equipment, and help achieve sustainability goals. Eaton employees around the world make a difference for their customers by creating an exceptional customer experience, solving problems with application expertise and developing innovative filtration solutions. Eaton’s filtration products are manufactured and sold worldwide. For more information, visit Eaton.com/filtration.

Eaton is an intelligent power management company dedicated to protecting the environment and improving the quality of life for people everywhere. We make products for the data center, utility, industrial, commercial, machine building, residential, aerospace and mobility markets. We are guided by our commitment to do business right, to operate sustainably and to help our customers manage power ─ today and well into the future. By capitalizing on the global growth trends of electrification and digitalization, we’re accelerating the planet’s transition to renewable energy sources, helping to solve the world’s most urgent power management challenges, and building a more sustainable society for people today and generations to come.

Founded in 1911, Eaton has continuously evolved to meet the changing and expanding needs of our stakeholders. With revenues of nearly $25 billion in 2024, the company serves customers in more than 160 countries. For more information, visit www.eaton.com. Follow us on LinkedIn.

Contact
Uta Hilgers
+49 6704 204 204