xStorage Home can be specifically useful when the maximum power consumption of the household is limited by the energy provider, for example through a utility contract.
Any consumption above the contracted maximum peak power consumption will be penalized and the homeowner will be charged accordingly.
With the xStorage Home peak-shaving mode, these additional energy costs can be avoided, since the excess energy consumption will be covered automatically by the xStorage Home system, charged either from the solar panels during the day or from the grid during times of low energy demand.