The i-on panel range has included the advanced functionality of the Web Browser Interface from the launch of the i-on40 in 2008. The WBI (Web Browser Interface) was initially integrated into the panel as a local programming tool; with the introduction of Eaton SecureConnect in 2017, Eaton is now able to deliver this handy and flexible tool via secure remote connectivity.
The WBI does not need any special software or a dedicated PC application; instead, it uses standard web browsers such as Edge or Chrome to display the interface. All smart devices such as mobile phones, tablets, laptops, or PCs have web browsers built into them which means they are compatible without the need to install dedicated software.
Using a standard web browser, all the panel configurations can be viewed or edited through simple drop-down lists, tick boxes, or text input fields, allowing a system to be completely programmed without using the local physical keypad. Locating the area of programming is made easy through the use of clear icons and menus. Configuration changes can be made easily and quickly without the need to wait for uploading and downloading as the WBI is a live interaction with the panel, so any changes made are applied instantly.
Part of the advanced functionality of the panel WBI is diagnostics providing an overview of crucial information such as any tampers, faults, and power status. Additionally, real-time feedback is provided on the status of zones, including if they have been recently activated and the current resistance values for the circuit. For radio devices and detectors, the last received signal strength can be reviewed.
As part of the WBI a Virtual Keypad (VKP) is included. This additional user interface allows complete access to the panel menus but with the familiarity of a physical keypad, providing an alternative method of remote programming for those more familiar with the layout of the keypad menus.
Another benefit of the WBI is the ability to back up the configuration, which provides the ability to save a file that is a carbon copy of how the panel is configured and what devices are connected to it. Should a panel be damaged or fail, using the restore facility of the WBI allows a panel to be restored to its original programming within minutes. Without this time-saving feature, the alternative would be the lengthy process of having to take to learn in all the devices and then manually programme the system.