NETTERSHEIM, GERMANY … Whether paints and coatings, chemicals, or process water – there are high requirements for the purity of liquid in numerous industrial applications. Filter bags made of polypropylene (PP) with defined nominal retention rates provide valuable services in safely retaining unwanted particles. However, sometimes an additional process step is required to absorb oil. To combine particle retention and oil absorption in a single process step, Eaton's Filtration Division has now launched the new SENTINEL® MAXPO and DURAGAF™ MAXPOXL filter bag ranges.
The fully-welded and with increased filter material thickness, SENTINEL MAXPO and DURAGAF MAXPOXL needle felt filter bags, made of PP, offer optimal particle removal with defined retention rates of 1 to 200 μm. Their design ensures easy handling, while an inner core, open on one side and comprised of a porous fiber matrix of pure, meltblown PP, serves as an internal pre-filter and enhances their filtration performance with powerful oil absorption. “This 2-in-1 function offers users the absorption performance of a cartridge filter and saves them an additional process step - and thus reducing costs and efforts in media treatment,” explains Wim Callaert, Senior Product Manager at Eaton’s Filtration Division.
The single open-end inner core is also less prone to blocking than other designs. Thanks to these and other design optimizations, the service life of the new filter bag ranges has been significantly increased. For applications where maximum capacity is required, DURAGAF MAXPOXL filter bags offer an additional two to five times longer lifespan thanks to a particularly thick extended-life filter material. “When capacity is reached, the fully-welded construction, along with practical handles on the bypass-proof SENTINEL sealing ring, makes it easier to change filter bags safely and cleanly,” continued Callaert.
The new SENTINEL filter bags from the MAXPO range and DURAGAF filter bags from the MAXPOXL range are now available. Both ranges are offered with nominal retention rates of 1, 5, 10, 25, 50 and 100 μm, SENTINEL filter bags are also available with a 200 μm retention rate. They are suitable for optimizing the filtration performance in a wide range of applications such as in water treatment, chemicals, paints and coatings, adhesives, petrochemicals and many more.
To achieve the optimal combination of quality, performance and safety, SENTINEL MAXPO and DURAGAF MAXPOXL filter bags can be inserted into Eaton's TOPLINE™ single bag and MAXILINE™ multi-bag filter housings. The flow through the side inlet on the top of the housing enables optimal sealing of the filter bags, easy replacement and reduces product loss to a minimum.
About Eaton’s Filtration Division:
Eaton’s Filtration Division is a leader in liquid filtration that can help companies improve product quality, increase manufacturing efficiency, protect employees and equipment, and help achieve sustainability goals. Eaton employees around the world make a difference for their customers by creating an exceptional customer experience, solving problems with application expertise and developing innovative filtration solutions. Eaton’s filtration products are manufactured and sold worldwide. For more information, visit Eaton.com/filtration.
Eaton is an intelligent power management company dedicated to protecting the environment and improving the quality of life for people everywhere. We make products for the data center, utility, industrial, commercial, machine building, residential, aerospace and mobility markets. We are guided by our commitment to do business right, to operate sustainably and to help our customers manage power ─ today and well into the future. By capitalizing on the global growth trends of electrification and digitalization, we’re accelerating the planet’s transition to renewable energy sources, helping to solve the world’s most urgent power management challenges, and building a more sustainable society for people today and generations to come.
Eaton was founded in 1911 and has been listed on the New York Stock Exchange for more than a century. We reported revenues of $23.2 billion in 2023 and serve customers in more than 160 countries. For more information, visit www.eaton.com. Follow us on LinkedIn.