ALTLUSSHEIM, GERMANY … The Filtration Division of intelligent power management company, Eaton, has expanded its product line with the launch of three high-performance filter series: the DUA, LWF, and DNR. The new filters are engineered to provide outstanding durability, efficiency, and reliability, making them ideal for demanding applications such as power generation, manufacturing, marine operations, and more.
“As pressures mount to safeguard critical processes and minimize downtime, having a dependable filtration solution that can operate uninterrupted is essential,” said Simone Ortner, Hydraulic Filtration Engineering and Product Manager at Eaton’s Filtration Division. “Our new filters are tailored to meet the practical needs of industries facing challenging conditions and tight operational schedules.”
New DUA Duplex Pressure Filters in ASME design
For nonstop, high-demand applications, Eaton’s DUA duplex filters build on the already available DU filter series, meeting ASME, PED and EN 13445 requirements without additional accessories. The DUA series also keeps filtration running smoothly by allowing the operator to divert the filtration flow from one side to the other. A clogging indicator can be assembled directly to the switch gear housing without any piping. Handling operating pressures up to 320 psi (22 bar) and flow rates of 1,056 gpm (4,000 l/min), DUA filters are ideal for power plants, manufacturing facilities, and marine systems. They are available in sizes 2005, 3005, and 4005.
New LWF In-line Pressure Filter Series
Eaton’s LWF in-line pressure filters are built for flexibility across various applications. They can be installed on suction, pressure, or return lines and are equipped with the pleated 01.E1501 filter element that boosts dirt-holding capacity. The filter element series features various filter media types and grades of filter finesse. The LWF series handles operating pressure up to 232 psi (16 bar), flow rates between 396 gpm (1,500 l/min) to 1,585 gpm (6,000 l/min) and is available in stainless steel (ELWF) as well as in ASME design (LWFA, ELWFA).
New DNR Duplex Pressure Filter Series
Eaton’s DNR duplex pressure filters are suitable for systems that need to withstand operating pressures up to 232 psi (16 bar). Designed with a three-way changeover valve, these filters allow for element changes without halting filtration and are well suited for lubrication of gear boxes and turbines. The carbon steel housing can hold Eaton’s 01.NR630 and 01.NR1000 filter elements, giving users flexibility across various setups and dependable performance under a range of conditions. The previously available DNR filter series is now available in sizes 5265 and 7265, and also includes a stainless-steel option (EDNR) as well as an ASME design (DNRA, EDNRA).
“By combining advanced design with different housing material options, these filters address the increasingly complex challenges of modern hydraulic and lubrication oil systems, ensuring optimal performance and peace of mind for their operators," adds Ortner.
Learn more about Eaton’s new DUA, LWF, and DNR filter series at eaton.com/filtration.
About Eaton’s Filtration Division:
Eaton’s Filtration Division is a leader in liquid filtration that can help companies improve product quality, increase manufacturing efficiency, protect employees and equipment, and help achieve sustainability goals. Eaton employees around the world make a difference for their customers by creating an exceptional customer experience, solving problems with application expertise and developing innovative filtration solutions. Eaton’s filtration products are manufactured and sold worldwide. For more information, visit Eaton.com/filtration.
Eaton is an intelligent power management company dedicated to protecting the environment and improving the quality of life for people everywhere. We make products for the data center, utility, industrial, commercial, machine building, residential, aerospace and mobility markets. We are guided by our commitment to do business right, to operate sustainably and to help our customers manage power ─ today and well into the future. By capitalizing on the global growth trends of electrification and digitalization, we’re accelerating the planet’s transition to renewable energy sources, helping to solve the world’s most urgent power management challenges, and building a more sustainable society for people today and generations to come.
Founded in 1911, Eaton has continuously evolved to meet the changing and expanding needs of our stakeholders. With revenues of nearly $25 billion in 2024, the company serves customers in more than 160 countries. For more information, visit www.eaton.com. Follow us on LinkedIn.