Download document () of 20
We make what matters work

LANGENLONSHEIM, GERMANY … Uncompromising filtration performance in challenging industrial applications—even at high flow rates—is what Eaton’s new TOPCART™ HF filter cartridge housings deliver. The single-filter cartridge housings are equipped with 20" or 40" restrainer baskets. Multi-filter cartridge housings are available in configurations for 4, 7, or 11 filter cartridges. The 20" version is only available in the 4-round configuration and is vertically oriented. The 40" and 60" versions are available in all multi-round configurations and are horizontally oriented to ensure easy and ergonomic cartridge replacement. All housings in the TOPCART HF range are designed for use with Eaton’s high-performance LOFPLEAT™ HF filter cartridges.

Suitable for a wide range of industrial applications in fine filtration—from pre-filtration before membranes to safety filtration and final product filtration—the filter cartridge housings can be configured to match the process requirements. The housings support a maximum operating pressure of 150 psi (10 bar) and temperatures up to 250°F (120°C). All variants of the TOPCART HF filter cartridge housings, including customized versions, are now commercially available. For specific applications, the housings are also available as engineered-to-order (ETO) solutions.

Bag-style performance with filter cartridge precision

The primary application of these housings is in industrial water treatment, such as cooling water systems, parts cleaning, and pretreatment for hydrogen production. Additional areas of use include the chemical industry, cooling or filtration applications in electronics and metal processing, oil and gas, data centers, power generation, and the pulp and paper industry. “These applications typically involve high flow rates, which would normally require a large number of standard filter cartridges. This increases the risk of contamination on the filtrate side during cartridge replacement. To address this, the housings are designed for high-flow cartridges that operate on the bag-style filtration principle while delivering the performance of traditional filter cartridges,” explains Ulrich Latz, Product Manager in Eaton’s Filtration Division. “The filtration direction is from the inside out, ensuring effective retention through the large, pleated filter surface area. When combined with LOFPLEAT HF filter cartridges, customers receive an ideal and complete, high-performance filtration solution from a single source,” Latz adds.

Ideal filtration results for industrial applications

With a high flow capacity of over 4,400 GPM (1,000 m³/h), the TOPCART HF filter cartridge housings are engineered for industrial applications with the highest performance demands. The use of high-quality stainless steel for all product-contacting components ensures that the housings meet all requirements even in harsh environments and with challenging media. The compact design, featuring an eye-bolt closure and glass bead-blasted surface, complies with all relevant standards and allows for integration into a wide range of industrial systems. Single- and multi-round versions are available with material certificates, specific testing requirements, ASME calculations, ASME U-Stamp certifications, and declarations of conformity according to the Pressure Equipment Directive (PED), if required.

eaton-topcart-hf-single-filter-cartridge-housing.jpg
TOPCART HF Single: The single-round version of the filter cartridge housing is available for 20" or 40" filter cartridges. The housing head with eye-bolt closure allows operators to easily replace the filter cartridge.
eaton-topcart-hf-multi-filter-cartridge-housing.jpg
TOPCART HF Multi: For high flow rates or particularly demanding filtration requirements, the filter cartridge housings are available in 4-, 7-, and 11-round configurations. The multi-round version is compatible with 20", 40", and 60" filter cartridges.
eaton-topcart-hf-multi-filter-cartridge-housing-detail.jpg
Four-round TOPCART HF Multi with LOFPLEAT HF filter cartridges: For secure placement and optimal filtration results, each filter cartridge is inserted into a restrainer basket. In the 40" and 60" versions, the horizontal design ensures ergonomic cartridge replacement.

About Eaton’s Filtration Division:

Eaton’s Filtration Division is a leader in liquid filtration that can help companies improve product quality, increase manufacturing efficiency, protect employees and equipment, and help achieve sustainability goals. Eaton employees around the world make a difference for their customers by creating an exceptional customer experience, solving problems with application expertise and developing innovative filtration solutions. Eaton’s filtration products are manufactured and sold worldwide. For more information, visit Eaton.com/filtration.

Eaton is an intelligent power management company dedicated to protecting the environment and improving the quality of life for people everywhere. We make products for the data center, utility, industrial, commercial, machine building, residential, aerospace and mobility markets. We are guided by our commitment to do business right, to operate sustainably and to help our customers manage power ─ today and well into the future. By capitalizing on the global growth trends of electrification and digitalization, we’re accelerating the planet’s transition to renewable energy sources, helping to solve the world’s most urgent power management challenges, and building a more sustainable society for people today and generations to come.

Founded in 1911, Eaton has continuously evolved to meet the changing and expanding needs of our stakeholders. With revenues of nearly $25 billion in 2024, the company serves customers in more than 160 countries. For more information, visit www.eaton.com. Follow us on LinkedIn.

Contact
Uta Hilgers
+49 6704 204 204