Select your location

Maintaining equilibrium in hydraulic systems

Explore how hydraulic systems find harmony in the flow of oil for different pressures.

In hydraulics, there is a loose rule that oil, under pressure, will take the easy way out! A little bit like human nature. If given the choice of an easy or difficult job, most people will take the easy route. There are ways of encouraging people to be more balanced in their approach by applying a restriction to the easier task, thereby encouraging an equal workflow for both the difficult and the simple. This is not dissimilar to hydraulics.

In a hydraulic system, flow takes place from high to low pressure, pressure being the result of restriction to the movement of the oil. If one actuator provides less restriction than another, then the former will move first. If the pressure to move the first actuator rises due to more restriction caused by the increasing flow, then the second actuator may start to move, but more slowly.

This can cause problems when two or more independent cylinders are required to move together. If they are unequally loaded, then the cylinder that provides the least amount of resistance will move first.

There are many machines that have this problem, both in linear and rotary movement, including transmission circuits. 

There are a number of answers to the problem, but one of the simplest and most cost- efficient is the humble spool-type flow divider. Unfortunately, misapplication of these valves can cause more system problems than solutions. In the first place, it is important to understand how these valves work. Figure 1 shows a section through a typical unit.

The valve functions as a flow divider and combiner by maintaining equal pressure drops through metering orifices situated in the two spools that are linked, in this case, by two ‘lugs’. In the division, mode the oil enters the valve through port ‘2’, passing through both spools and out of ports ‘1’ and ‘3’. The oil passes through the control orifices in the spools, and if the flow is equal, the spools remain in the central position as shown. If, due to a change in outlet pressure, there is a tendency for more oil to pass through one side than the other, then the pressure drop rises in that side, causing it to drag the other spool across, thereby eventually restricting the outlet of the higher flow side while keeping the lower flow side open.

As soon as the pressure drop through the control orifice in both spools is equal, the assembly will maintain a metering position that keeps the flow from both legs equal. Any change in the outlet pressures will cause the spool to move, accommodating the change by metering the oil through the path of least resistance.

When the valve is being used as a combiner, the spools will be pushed together as shown in Figure 2. The oil then flows through the same orifices in the other direction, combining out of port ‘2’. When there is a change in equilibrium, the spools push each other to restrict the line of least resistance.

The accuracy of the valve depends on the size of the two orifices, the spring force and the leakage across the spools. If the tolerances on these items are kept to a minimum, accuracies of +/- 3% can be achieved.

Most production valves state an accuracy of +/- 10% on inlet flow. In some applications, this can cause problems when the cylinders are not flexible enough to accommodate this inaccuracy.

With this kind of design, there is also a minimum flow at which the valve will operate. The relationship between the orifice diameter and the spring force opposing the movement of the spool means that there is a minimum flow before the spool will move and start to compensate.

If, for some reason, the flow from either leg is restricted, then the spools will react to the offset pressure drops, causing the spools to move to one end of the cartridge and to block off both outlets. This can be overcome by placing relief valves down stream of the flow divider to allow the flow to continue through a blocked or restricted outlet.

In cylinder applications, the cylinders may not reach the end of stroke together. There will be a small make-up flow, but if relief valves are used, the slower leg will catch up at 50 % of the inlet flow. There are versions of flow dividers that have extra holes to increase the make-up flow. These, however, become less accurate as the pressure difference between the two legs increases.

It is not necessary to fit flow dividers of this type on the inlet and outlet lines. The flow divider combiner will maintain equal division in both directions, but care must be taken to size the flow divider to suit the outlet flow if it is in the full-bore side of the cylinder, as the flow will be increased by the rod/bore ratio of the cylinder.

It is not practical to cascade these valves to control more than two cylinders because the inaccuracy of the valves will be additive, meaning you could end up with a 20 to 30 % difference in the flow. 

It is also important that the valves are not over-flowed. When in the dividing mode, the pressure drop through the spools acts directly on the ‘lugs’ and rips the two spools apart. The normal factor of safety is 4:1 on ultimate tensile strength, and since the pressure drop through an orifice rises as the square of the increase in flow, putting twice the rated flow through the valve will produce four times the pressure drop and probably break the ‘lugs’ The normal and most common division ratio is 50/50, but it is possible to produce offset ratios by means of different diameter orifices in the opposing spools. The ratio of the orifice area in each spool will determine the offset flow ratio.

In spite of these draw backs, there are many applications where the performance is good enough and therefore offers a cost-effective solution to the problem of providing effective division of flow, despite varying pressures in each actuator.

The accuracy of the valve depends on the size of the two orifices, the spring force and the leakage across the spools.

A typical example is on the arms of a tarpaulin cover for tipping trucks. The arms, on either side of the lorry, have to extend together first and then rotate together to unroll the tarpaulin and stretch it over the insecure load in the skip.

One of the most common applications for flow dividers are wheel motors in transmission circuits, to give an element of ‘diff-lock’. The flow divider will ensure that there is always traction to both wheels, even when one of them is on soft or slippery ground.

Figure 3 shows a typical circuit where the flow divider is switched in when needed. The flow divider works on pressure drop and is thus intrinsically inefficient, even though the pressure drop is low. In a transmission circuit, this pressure drop would create excessive heat, making it necessary to have a system for selecting the diff-lock when required.

The accuracy of the valve depends on the size of the two orifices, the spring force and the leakage across the spools.

A typical example is on the arms of a tarpaulin cover for tipping trucks. The arms, on either side of the lorry, have to extend together first and then rotate together to unroll the tarpaulin and stretch it over the insecure load in the skip.

One of the most common applications for flow dividers are wheel motors in transmission circuits, to give an element of ‘diff-lock’. The flow divider will ensure that there is always traction to both wheels, even when one of them is on soft or slippery ground.

Figure 3 shows a typical circuit where the flow divider is switched in when needed. The flow divider works on pressure drop and is thus intrinsically inefficient, even though the pressure drop is low. In a transmission circuit, this pressure drop would create excessive heat, making it necessary to have a system for selecting the diff-lock when required.

In a closed-loop transmission circuit, this can be achieved by using logic elements around each side of the flow divider. 

They are vented when the diff-lock is not required. This will work in both directions because the charge-pump pressure is sufficient to keep the logic element vented, allowing the flow to pass backwards through the valve.

The bypass can be achieved by using pilot-operated spool valves or solenoid valves. When using one of these options there is no loss of flow through the vent line, but there is a limit to the flow rate that these kinds of valves can handle.

Most of these machines are required to go around corners, so that one wheel has to go faster than the other. As previously described, this would cause problems to the flow divider. It is also true that it is not necessary to maintain a perfect division under conditions requiring diff-lock. A limited slip differential is acceptable.

It has become commonplace to fit an orifice across the two legs of the flow divider to allow flow to pass from one side to the other when the vehicle is turning. As the differential pressures go up due to the extra load on the inner wheel, a controlled flow can pass from one side to the other. The size of this orifice depends on the turning circle of the machine. In this way, one wheel will be able to move faster than the other, but pressure and therefore torque will remain on both of the wheels.

There are a number of different designs of flow divider on the market, including valves that have a wider range of flow. This can be an advantage if the inlet flow varies from very low to the maximum rating of the valve, but at low flows, there will still be an inaccuracy. Some designs can cope with very low flows, but as with all flow dividers, they are not 100 % accurate and can cause more problems than they solve. At low flows, the standard spool-type flow divider will function as a simple “T" connector, and it is sometimes preferable to use this feature at low flow rates and then gain their benefits at higher rates.

Gear flow dividers are also available. These do not work in the same way; they are essentially two gear pumps/motors working in parallel on the same shaft. Each section will rotate at the same speed, so that the outlet flows remain constant from each leg. Their accuracy depends on the leakage across the gears and is thus much better than that of the spool type. It is very important that relief valves are fitted to the outlet legs because if one leg meets a restriction, the other legs will transmit their torque to the stalled line and intensify the pressure. If the gear flow divider has two sections, the pressure could double in the stalled line. If three sections are used this pressure will triple. They do not suffer from the same pressure-drop problem but are significantly more expensive.

Another way of maintaining equal movement on cylinders is the use of slave cylinders, in which a number of double-acting cylinders are securely and rigidly connected together at both the rod and barrel and have a common inlet. Each outlet is connected individually to the inlet of the main working cylinders. (Obviously, some provision for filling and maintaining the oil in the main cylinders has to be made.) As oil enters the common inlet of the slave cylinders, the rods will extend together, displacing fluid from each cylinder equally, which operates the main working cylinders. This is a far more accurate way of controlling multiple cylinders, but requires a more complicated control circuit and much more space.

A simple way of improving the accuracy and keeping the price down is to use restrictive-style, pressure-compensated flow regulators mounted in parallel. It is important that there is always more flow available than the combined settings of the flow regulators. This solution requires the excess flow to go across a relief valve, but it can be used successfully with a pressure compensated pump. Each valve can be trimmed to give optimum performance.

The spool flow divider may appear to have a number of drawbacks, but if the aim is to maintain cylinder or motor equilibrium in a cost-effective manner it is worth a look. Taking into account the point made previously, proper application will give good results.