Dokumentum letöltése () 20
Működésbe hozzuk az igazán fontos dolgokat.*
oil.jpg

Location Details: Western Australia

Problem: Maximize use of scarce water resources and improve flow rates for injection pumping systems

Solution: TOPLINE Filter Housings with 10 micron SENTINEL Filter Bags.

Results: Achieved flow rate to the required rate of 100 m3/min. with capacity to spare for potential expansion

Background

A challenge faced by a petroleum producer in Western Australia was how to bring oil to the surface when there was insufficient pressure in the crude oil reservoir below ground. A water injection system, where water is pumped back into the reservoir to increase pressureand thereby stimulate production, was installed. Normally only 30% of the oil in a reservoir can be extracted, but with water injection that percentage increases. Because of the desert location the water in the system has to be filtered and recycled to keep consumption to a minimum. Over time the water flow rate required by the application exceeded thecapacity of the filtration system.

Solution

The existing filtration system consisted of “home-made” filter bag housings with 50 micron filter bags that fed into 10 micron cartridge filters. This system could not provide an adequate flow of water for the application and because of the cartridges, the operating costs were high. Eaton’s solution was to completely replace the existing filtration systems with a bank of six TOPLINE Filter Housings with 10 micronSENTINEL Filter Bags. Differential pressure gauges were fitted to the filter housings to indicate when filter bag changes were required.

Result

The Eaton system, with a design flow rate of 200 cubic meters per hour was more than adequate to handle the applications requirement of 100 cubic meters per hour and would be able to meet future requirements as well. The system operators were pleased because the new system was easier to operate and maintain than the older one. And, without the cartridges, it was less costly. After running successfully for several months the customer began looking at other locations where this system or a similar one could be used.

TOPLINE
Eaton TOPLINE single bag filter
SENTINEL Filter Bags
Eaton SENTINEL filter bags
topline-oil-filter.jpg
Bank of six TOPLINE housings process up to 200 cubic meters per minute