Select your location

Eaton’s new CMT mobile valve section increases design flexibility, reduces valve bank size with two-service control capability

May 20, 2020

EDEN PRAIRIE, Minn. … Power management company Eaton today announced the launch of the CMT mobile valve section, a streamlined new section option for the CMA advanced mobile valve. With the capability to control two bidirectional services from one section—an industry first—the CMT valve section increases design flexibility and reduces CMA valve bank size, weight and overall system cost.

Like the existing CMA mobile valve section, the new CMT section is software-configurable and features CAN communication, onboard sensors, digital flow-sharing and electronic load-sensing to provide precise flow control and high responsiveness. While the CMA section features independent metering, the CMT section utilizes the twin-spool architecture to control two services instead of one. This can reduce the total number of sections needed in a valve bank by as much as 50 percent, minimizing valve bank size and weight.

CMT mobile valve sections are stackable with CMA sections, which increases the design flexibility of the CMA advanced mobile valve. Original equipment manufacturers (OEMs) can optimize the valve for all vehicle requirements by specifying sophisticated CMA sections for services that demand superior precision and control and streamlined CMT sections for standard machine functions. The availability of two stackable section options simplifies the use of the CMA valve on high-end and midrange machines without parts proliferation, due to shared componentry and procedures.

“The new CMT mobile valve section reduces overall system cost without sacrificing performance,” said Todd Degler, global product manager, Advanced Mobile Valves, Eaton. “OEMs can merge the next-generation performance of CMA sections with value-oriented CMT sections to create the optimal valve solution for new mobile machinery designs.”

The CMA advanced mobile valve significantly improves machine performance and operator productivity. Featuring onboard electronics and sophisticated software algorithms, the CMA valve can optimize for conditions such as oscillation and vibration to deliver better stability, controllability and fuel efficiency. Software-driven setup eliminates hardware changeouts and enables performance optimization in minutes instead of months, speeding time to market.

To learn more about the CMA advanced mobile valve and CMT mobile valve section, visit Eaton.com/CMA and Eaton.com/CMT

Eaton’s mission is to improve the quality of life and the environment through the use of power management technologies and services. We provide sustainable solutions that help our customers effectively manage electrical, hydraulic, and mechanical power – more safely, more efficiently, and more reliably. Eaton’s 2019 revenues were $21.4 billion, and we sell products to customers in more than 175 countries. We have approximately 95,000 employees. For more information, visit Eaton.com.

Contact
Lindsay Schleisman, 952-937-7462