Select your location

GALESBURG, Mich. … Power management company Eaton today introduced new “wet kit” packages for end-dump applications supporting the Bezares line of Power Takeoff (PTO) units that fit popular Eaton Fuller® and Eaton Cummins Endurant™ transmissions. Bezares SA is a global manufacturer of PTOs, hydraulic pumps, fittings, tanks, valves and other related mobile power hydraulic components.

The wet kits simplify ordering by including all the components needed into a single part number. Wet kits are installed on medium- and heavy-duty trucks with accessories such as booms and cranes that need hydraulic pumps to operate. The wet kit’s hydraulic pump is activated by the truck's transmission.

Each wet kit includes a PTO with Viton® seals and Garlock® gaskets for easier installation and fewer leaks, a high-quality roller bearing dump pump for reliability, and an aluminum tank for lighter weight. Compiling all the needed components in one kit streamlines installation, which saves time when compared to ordering a system with individual parts and numbers.

“Eaton’s PTO wet kits are a simple solution to a complex problem that provides our customers with a turnkey solution for end-dump applications,” said Tim Bauer, vice president, Aftermarket, Eaton’s Vehicle Group. “Our goal is to make life easier for users by providing everything they need. We’ve already done the homework for them.”

Many of the kit’s components allow end users to configure the hydraulic systems to individual customer or application needs, such as a 50-gallon aluminum tank, which can be mounted either behind the cab or with a round side mount. A direct-mount air shift dump pump can be used with both two- and three-line systems.

The kits are immediately available for shipment and can be ordered through Eaton mobile power distributors. All kits come complete with all the hardware and components needed for seamless installation. Additional information on Eaton’s PTO Wet Kit.

Eaton reached a distribution agreement with Bezares SA in 2019 to become the North American master distributor for its mobile power hydraulic portfolio. In addition to distribution services, Eaton also provides post-sale service and support for the PTOs through its extensive Roadranger® field team.

Eaton’s mission is to improve the quality of life and the environment through the use of power management technologies and services. We provide sustainable solutions that help our customers effectively manage electrical, hydraulic, and mechanical power – more safely, more efficiently, and more reliably. Eaton’s 2019 revenues were $21.4 billion, and we sell products to customers in more than 175 countries. We have approximately 93,000 employees. For more information, visit www.eaton.com.

Contact

Thomas Nellenbach
thomasjnellenbach@eaton.com
(248) 226-6852 (office)
(216) 333-2876 (cell)

Eaton wet kit packages for end-dump applications
Eaton’s new “wet kit” packages simplify ordering by including all the Power Takeoff (PTO) components needed for end-dump applications into a single part number.