Download document () of 20
We make what matters work*

Thermal cycler/DNA cycler

Thermal cyclers (also known as DNA cyclers, thermocyclers, PCR machines or DNA amplifiers) are used to amplify segments of DNA via the polymerase chain reaction and are essential for labs that rely on molecular biology. Their use is crucial for applications such as detection and diagnosis of infectious diseases and hereditary diseases, DNA cloning for sequencing and DNA profiling. Thermal cyclers provide a thermally controlled environment for DNA samples that are necessary during temperature cycling. Because the process relies heavily on precise temperature control, it is vital that this equipment has proper thermal management. Because they required the best possible thermal design for their newest Thermal cycler design, Bio-Rad contacted Eaton.

In order to perform with peak accuracy, uniformity and speed, the thermal optimization of the product needed to be designed with a heat sink configuration that maintained less than +/-0.5°C variation in temperatures from sample to sample.

Eaton also needed to determine the feasibility of removing edge heaters from the sample block by recommending an appropriate insulation scheme and thermal interface materials.

Eaton engineers evaluated several fan and heat sink combinations by creating airflow-thermal simulation models to choose a particular fan, number of fans, location of fans, heat sink geometry, etc. These simulations helped in the selection of an optimal combination of fan and heat sink. The team then created a prototype of the unit to capture all heat and airflow related details. The prototype was tested for temperature variation and the data was used to enhance the accuracy and reliability of simulation predictions.

To further optimize the overall product design, Eaton engineers evaluated the feasibility of removing heaters used to minimize the sample to sample temperature variation. It was shown using simulations that placing polyurethane foam at key locations can maintain the sample to sample temperature variation without the side heaters.

Bio-Rad utilized the recommended Eaton solution and implemented it into their thermal cycler design, which is still being produced today. This Bio-Rad thermal cycler has now been in use for several years with excellent results. Over the years, the final products have maintained their accuracy and reliability and Bio-Rad is known for their robust, high performing PCR amplification equipment.

Heat sink solutions