When it comes to cybersecurity, safeguarding power equipment may not always rank top of mind. Yet with hackers relentlessly exploiting new devices in innovative ways, coupled with more employees working remotely than ever before, vulnerabilities are emerging that you may not have previously considered. Because infrastructure equipment is smarter and more interconnected than ever before, deploying an end-to-end cyber defense solution has become absolutely essential.
Eaton uniquely understands the severity of threats faced by today’s organizations and how to best protect yourself from cybersecurity attacks. We’ve developed an entire portfolio of products with ingrained measures to prevent intrusion and mitigate risks. While there are different ways to address both cyber and physical security in power equipment, our solutions work in harmony to provide resilient, layered protection that help keep your operations and personnel safe.
Endpoint device security is the top concern of IT pros for their remote workforce.
Eaton has always taken a multi-faceted and industry-leading approach to cyber defense that differentiates us from our competitors. Several years ago, we established our own Cybersecurity Center of Excellence. This alliance is designed not only to drive standards, best practices and technology across the enterprise, but also to be a resource hub to help customers to develop more security awareness and solve cybersecurity challenges.
As organizations rapidly pursue digital transformation and adopt new technologies and business processes, security issues are on the rise. In fact, 85 percent of CISOs reported that security concerns during digital transformation had a "somewhat" to "extremely large" business impact. This is especially true for companies that lack integration across their security solutions and complete visibility into user, system and network behavior. Software and power systems must work together to ensure a cohesive, seamless and layered protection solution for optimal network security against computer malware and other attacks.
As organizations attempt to juggle the challenges of shrinking budgets, mobile workforces and requirements to do more with less, they must also pause to consider the possible ramifications of a cybersecurity breach: What would the cost be? How would operations be impacted? Could the business survive? While antivirus and malware software represents a starting point, it is critical to maintain an end-to-end, holistic view of cybersecurity that encompasses every aspect of an organization’s power system.
Firmware updates are essential
Gigabit Network Card ── The industry’s first UPS network card with built-in cybersecurity features UL 2900-1 and IEC 62443-4-2 certification, with stronger encryption, configurable password policy and usage of CA and PKI signed certificates.
IPM software ── Ensures uptime and data integrity with centralized power resource management while keeping data safe through graceful, sequential shutdown. IPM enables complete management of firmware updates.
Metered and Managed rackmount PDUs ── Simplifies load balancing and decision-making based on energy consumption through real-time monitoring, plus reboots connected loads with remote on/off switching (managed models) and turns off unused outlets to prevent unauthorized access (managed models).
TANlock by Eaton ── Keeps unwanted guests out of rack enclosures with two-factor authentication options, as well as monitors and manages access credential logins to provide access to specific individuals.
Rack enclosures ── Secure IT devices in sturdy 4-post racks enclosures featuring highly secure combination locks.
MiniRaQ by Eaton ── Secures IT equipment in a wallmount rack with a locking lid, heat removal, air filtering and data/cable management accessories.
Think today’s cyber criminals make entry solely through vulnerable computer systems? Think again. Unfortunately, hackers are constantly coming up with new and innovative ways to infiltrate your devices, many of which lack the security features that are standard in computers, tablets and even smartphones. From household appliances to medical equipment, a growing list of equipment poses a serious threat to system-crippling cybercrime. We’ve compiled five of the most shocking:
Internet-connected security cameras on home networks account for almost half of the IoT devices compromised by hackers, according to research from cybersecurity company SAM Seamless Network.
Although baby monitors began as simple one-way radio transmitters, over the years they have evolved into sophisticated Wi-Fi enabled smart devices complete with features such as cameras and infrared vision. Unfortunately, the IoT devices aren’t smart enough to thwart hackers; in late 2018, a cyber crook accessed the wireless camera system in a U.S. monitor and threatened to kidnap the baby. Meanwhile, there are multiple reported incidents of strangers’ voices being heard over baby monitors.
Although Gartner estimates there will be more than 20 billion IoT devices by 2020 ── and as many as 75 billion by 2025 ── the safety of these devices is still widely ignored.