Download document () of 20
We make what matters work*

Extruded heat sinks

Extruded heat sinks are one of the most popular types of heat sinks. They’re easy to make in bulk, economical and have fewer secondary operations before a final product than other heat sink technologies. That’s why the extrusion process is so widely used in other applications like window frames and door jams, pipes and tubing and food like pasta and French fries. Extrusion is straightforward and in the thermal management industry, it’s easy for us to take advantage of this technology.

Extrusions and extruded heat sinks: how they’re made

From billet to profile

In the aluminum extrusion process, the metal in a billet form is heated up to the point where it’s soft enough where it can squeeze through the extrusion die, but not so soft where it’s molten and would drip out. The hydraulic press pushes a ram into the billet which forces the aluminum through the heavily engineered extrusion die. This die is the cross section or aluminum extrusion profile the long extrusion will have.

Engineers carefully design extrusion dies so they produce the required shape, but can still withstand the pressure of the aluminum billet being pressed against it without breaking. This is especially true for heat sink dies since there are lots of fingers for the fin gaps which could break off from the die. Too much aluminum pressing on long thin fingers will easily snap them off and destroy the die.

Extrusion stretching

After the aluminum is extruded out, it’s pulled along the run out table where it is straightened and allowed to cool. When first manufactured, these bars can be upwards of hundreds of feet long. For ease of shipping and manufacturing purposes, the giant lengths are then cut into more manageable lengths, typically around 8 feet.

From raw bar to extruded heat sinks

From here, these aluminum extrusions are then cut to length for the application they will be used in. Any sort of machining, holes or other features are machined into the extrusion to customize it as necessary. This is also when finishing, like anodizing or painting, occur to finish off the heat sink. 

Eaton heat sink chromate finish
Check out our Aluminum extrusion profiles, air-cooled Extruded heat sinks or specialty, Max Clip™ extrusions. Contact us to learn about our extrusion options.